Clock
Features Supported
Provide system tick functionality using a single timer to periodically interrupt the CPU
Default tick period is 1000 usecs
Using this system tick,
Users can create arbitrary number of clock objects
When a clock object expires, a user specified callback is called
Clock expiry time is specified in units of clock ticks
Each clock can be started in one-shot callback or periodic callback mode
Provides APIs to wait ‘n’ clock ticks, get current clock ticks
Provides APIs to convert clock ticks to time in usecs and vica versa
API to get current time in units of usecs
Features NOT Supported
NA
Important Usage Guidelines
The user specific callback can be called in interrupt, SWI or task context depending on the underlying RTOS that is used
In no-RTOS case, the callback is called in interrupt context
It is recommended to assume that the callback is called in ISR context and not block within the callback.
Typically one should do very limited work within the callback itself and defer the larger part of the work to a task via a semaphore post.
ClockP_usleepandClockP_sleepwill block until the user specified time is expired.In no-RTOS case, there is only a single main task and that will block or spin until the ticks have elasped
In RTOS case, the current executing task will ‘pend’ and schedular will switch to another ready task
In both cases ISR’s are still active
In RTOS case, actual sleep will be in the range of
sleep time - ClockP_ticksToUsec(1)tosleep time. If you need to guarantee atleast minimum sleep ofsleep time, you need to sleep forsleep time + ClockP_ticksToUsec(1), i.e there will be a error on 1 OS tick at max.
When using multiple CPUs, make sure each CPU uses a different HW timer else the tick ISR will not trigger as expected.
Recommended value of tick period is 1ms or 1000us
Adding any module in SysConfig, automatically adds a clock module with a timer configured for 1ms. The default timer is chosen such that it does not overlap with a timer from another CPU.
In M4F, the M4F internal SysTick timer is used.
In R5F, one of the many SOC level timer is used.
Example Usage
Include the below file to access the APIs,
Example callback that increments a global counter based on the clock that invoked the callback:
Example usage to create a clock in one shot mode with timer expiry of 10ms:
Example usage to create a clock in periodic mode with timer period of 100ms:
Example usage to measure time and profile a function:
API Reference
Defines
-
ClockP_OBJECT_SIZE_MAX
Max size of clock object across no-RTOS and all OS’s.
Typedefs
-
typedef void (*ClockP_FxnCallback)(ClockP_Object *obj, void *args)
Callback that is called when the clock expires.
- Param obj:
[in] Clock object associated with this callback
- Param args:
[in] user specific argument pointer that was passed via ClockP_Params
Functions
-
void ClockP_init(void)
Initialize the clock module.
The API is called during system init to setup a timer to run at a periodic time internval of ‘n’ micro seconds.
‘n’ can be configued by the user via SysConfig, default value for ‘n’ is typically 1000 us
Using this single timer, the clock API can be used to start multiple ‘clock’s in units of clock ticks.
-
void ClockP_deinit()
De-initialize the clock module.
This API is called at the end of the application to stop timers and destroy interrupt handlers
-
void ClockP_Params_init(ClockP_Params *params)
Set default values to ClockP_Params.
Strongly recommended to be called before seting values in ClockP_Params
- Parameters:
params – [out] parameter structure to set to default
-
int32_t ClockP_construct(ClockP_Object *obj, ClockP_Params *params)
Create a clock object.
when ClockP_Params.start = 1, this also starts the clock object
- Parameters:
obj – [out] created object
params – [in] parameter structure
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE on error
-
void ClockP_destruct(ClockP_Object *obj)
Cleanup, delete, destruct a clock object.
- Parameters:
obj – [in] object
-
void ClockP_start(ClockP_Object *obj)
Start the clock, if not already started.
If clock is already started, then this restarts it with updated timeout and period, if any.
- Parameters:
obj – [in] object
-
void ClockP_stop(ClockP_Object *obj)
Stop the clock, if not already stopped. No effect if clock is already stopped.
- Parameters:
obj – [in] object
-
uint32_t ClockP_isActive(ClockP_Object *obj)
Check if clock is active i.e not expired.
For clock setup in periodic mode, clock will always be active after it is started and before it is stopped.
For clock setup in one-shot mode , clock will be active after it is started and will be inactive after clock expires or it is stopped.
- Parameters:
obj – [in] object
- Returns:
0: clock is not-active or expired,
1: clock is active or not expired
-
void ClockP_setTimeout(ClockP_Object *obj, uint32_t timeout)
Set clock timeout value, takes effect for next clock start.
- Parameters:
obj – [in] object
timeout – [in] clock expiry period of first clock execution, in units of clock ticks
-
uint32_t ClockP_getTimeout(ClockP_Object *obj)
Get current remaining time in units of ticks.
- Parameters:
obj – [in] object
- Returns:
clock expiry period of next clock execution, in units of clock ticks
-
uint32_t ClockP_getTicks(void)
Get current clock ticks.
- Returns:
number of clock ticks that have elasped since ClockP_init()
-
uint64_t ClockP_usecToTicks(uint64_t usecs)
Convert usecs to clock ticks.
- Parameters:
usecs – [in] time in micro seconds
- Returns:
nearest integer clock ticks
-
uint64_t ClockP_ticksToUsec(uint32_t ticks)
Convert clock ticks to usecs.
- Parameters:
ticks – [in] number of clocks ticks
- Returns:
nearest integer micro seconds
-
uint64_t ClockP_getTimeUsec(void)
Get current time in units of usecs.
-
void ClockP_usleep(uint64_t usec)
Sleep for user specified usecs.
Note
Actual sleep will be in the range of
usec - ClockP_ticksToUsec(1)tousec. If you need to guarantee atleast minimum sleep ofusec, you need to sleep forusec + ClockP_ticksToUsec(1).- Parameters:
usec – [in] Time to sleep in units of usecs
-
void ClockP_sleep(uint32_t sec)
Sleep for user specified seconds.
Note
Actual sleep will be in the range of
sec - ClockP_ticksToUsec(1)tosec. If you need to guarantee atleast minimum sleep ofsec, you need to sleep forsec + ClockP_ticksToUsec(1).- Parameters:
sec – [in] Time to sleep in units of secs
-
struct ClockP_Object
- #include <ClockP.h>
Opaque clock object used with the clock APIs.
Public Members
-
uintptr_t rsv[ClockP_OBJECT_SIZE_MAX / sizeof(uint32_t)]
reserved, should NOT be modified by end users
-
uintptr_t rsv[ClockP_OBJECT_SIZE_MAX / sizeof(uint32_t)]
-
struct ClockP_Config
- #include <ClockP.h>
ClockP module config, set as part of SysConfig, not to be set by end-users directly.
Public Members
-
uint32_t timerBaseAddr
HW Timer MMR base address
-
uint32_t timerHwiIntNum
CPU interrupt number for this timer
-
uint32_t eventId
-
uint32_t timerInputClkHz
Timer clock in units of Hz
-
uint32_t timerInputPreScaler
Timer divider to apply to the input clock
-
uint32_t usecPerTick
period of one timer tick in units of usecs
-
uint32_t timerBaseAddr
-
struct ClockP_Params
- #include <ClockP.h>
Parameters passed during ClockP_construct.
Public Members
-
uint32_t start
0: do not start the clock after construct,
1: start the clock after construct
-
uint32_t timeout
clock period for first execution, in units of clock ticks
-
uint32_t period
clock period for subsequent periodic execution, in units of clock ticks.
Set to 0 for one-shot mode of operation
-
ClockP_FxnCallback callback
User callback to invoke when timer expires.
Note
Callback could be called in ISR context, so user should not block within the ISR
-
void *args
User argument that is available inside the callback
-
const char *name
Name to associate with this object
-
uint32_t start