Release Notes 11.01.00

Attention

Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.

Note

The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination. Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC

Supported CPUs

EVM

Host PC

AM62P

MCU R5F, WKUP R5F

SK-AM62P-LP EVM (referred to as am62px-sk in code)

Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Feature

Module

ECC Functional Test example for single bit errors is added

SDL

Updated DDR configuration from DDR configuration tool v10.30

DDR

Experimental Features

Attention

  • Features listed below are early versions and should be considered as “experimental”.

  • Users can evaluate the feature, however the feature is not fully tested at TI side.

  • TI would not support these feature on public e2e.

  • Experimental features will be enabled with limited examples and SW modules.

Feature

Module

Ethernet traffic sharing accross multiple cores, called Ethernet Firmware

Networking

Dependent Tools and Compiler Information

Attention

It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.

Tools/Components

Supported CPUs

Version

Code Composer Studio

MCU-R5F, WKUP-R5F

20.2.0

SysConfig

MCU-R5F, WKUP-R5F

1.24.0, build 4150

TI ARM CLANG

MCU-R5F, WKUP-R5F

4.0.1.LTS

GCC AARCH64

A53

9.2-2019.12

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

11.1.0

SDK Components

SYSFW / TIFS

Version 11.01.02
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS

Supported CPUs

SysConfig Support

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

NA

FreeRTOS POSIX

MCU-R5F

NA

No RTOS

MCU-R5F, WKUP-R5F

NA

Driver Porting Layer (DPL)

Module

Supported CPUs

SysConfig Support

OS support

Address Translate

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Cache

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Clock

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

CycleCounter

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Debug

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Heap

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Hwi

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

MPU

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Semaphore

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Task

MCU-R5F, WKUP-R5F

NA

FreeRTOS

Timer

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode

Supported CPUs

SysConfig Support

PHY Support

DMA Support

OS support

OSPI NOR

WKUP-R5F

Yes

Yes

Yes

NORTOS

EMMC

WKUP-R5F

Yes

NA

NA

NORTOS

UART

WKUP-R5F

Yes

NA

No

NORTOS

SDL

SDL Module

Supported CPUs

SysConfig Support

MCRC

MCU-R5F

No

ESM

MCU-R5F

No

VTM

MCU-R5F

No

DCC

MCU-R5F

No

ECC

MCU-R5F

No

RTI

MCU-R5F

No

POK

MCU-R5F

No

STOG

MCU-R5F

No

MTOG

MCU-R5F

No

PBIST

MCU-R5F

No

LBIST

MCU-R5F

No

ROM_CHECKSUM

MCU-R5F

No

Networking

Module

Supported CPUs

SysConfig Support

OS Support

Key features tested

Key features not tested

TSN

WKUP-R5F

NO

FreeRTOS

gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration

Multi-Clock Domain

LwIP

WKUP-R5F

YES

FreeRTOS

TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver

Other LwIP features

Ethernet driver (ENET)

WKUP-R5F

YES

FreeRTOS

Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW

RMII mode

SOC Device Drivers

Note

See the updated MCASP usage guidelines in MCASP for changes in MCASP driver

Peripheral Domain Supported CPUs SysConfig Support
DDR Main WKUP-R5F Yes
ECAP Main MCU-R5F Yes
EPWM Main MCU-R5F, WKUP-R5F Yes
DSS Main WKUP-R5F Yes
GPIO MCU MCU-R5F, WKUP-R5F Yes
Main MCU-R5F, WKUP-R5F Yes
I2C Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
IPC Main MCU-R5F, WKUP-R5F Yes
MCAN MCU MCU-R5F Yes
MCASP Main WKUP-R5F Yes
MCSPI Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Pinmux Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
SOC NA MCU-R5F, WKUP-R5F Yes
SCIClient NA MCU-R5F, WKUP-R5F Yes
UART Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup WKUP-R5F Yes

Fixed Issues

ID Head Line Module Applicable Releases
EXT_EP-12721 ECC TCM example cannot be built for AM62P SDL 11.01.00
EXT_SITMPUSW-97 SBL_SD_LINUX fails to initialize SD card if booted over any media except SD card SBL 09.02.00
EXT_SITMPUSW-103 AM62P - MCU+SDK 11.0 fails to compile on Windows Build 11.00.00
EXT_SITMPUSW-105 MMCSD driver uses snprintf function from libc MMCSD 11.00.00
EXT_SITMPUSW-77 Modify Read capture delay logic for Tap Mode OSPI 11.00.00
EXT_SITMPUSW-106 OSPI Phy Tuning Data is not written correctly in Flash_norOspiOpen() OSPI 10.01.00

Known Issues

ID Head Line Module Reported in release Workaround
EXT_SITMPUSW-1085 Flash_eraseSector and Flash_norOspiEraseSector does not erases the mentioned sector. Flash 11.00.00 No known workaround
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC 08.03.00 No known workaround
EXT_SITMPUSW-109 Wrong comments on HwiP_inISR() API DPL 11.00.00 No known workaround
EXT_SITMPUSW-78 MMCSD Sysconfig provides options to configure PHY type MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-84 MMCSD error recovery sequence isn't implemented correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-110 eMMC Init Code Missing DLL Register Settings needed for Initial Legacy SDR Mode Phase MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-113 eMMC PHY I/O Calibration not getting executed during eMMC boot MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-123 MMCSD driver does not follow the SWITCH command sequence correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-124 EXTCSD HS_TIMING register is set incorrectly at certain places in the driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-125 MMCSD driver uses infinite loop instead of timeout for checking fields of PRESENTSTATE register MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-126 Timing issues with MMCSD host controller driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-127 Incorrect handling of the CAPABILITIES register in the eMMC initialization MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-128 EMMC timiing parameters to be changed based on SOC and MMC instance MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-137 Random CRC errors observed for eMMC HS400 mode on random reset test MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-138 MMCSD_read & MMCSD_write function are not designed simple & readable MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-139 Comment and Implementation does not match in the MMCSD_retune MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-117 Linux Kernel IPC Examples are broken IPC 11.00.00 Change ti.ipc4.ping-pong to rpmsg-client-sample in the example
EXT_SITMPUSW-121 FORCE bit not book keeped properly for MCSPI DMA mode of operation MCSPI 11.00.00 No known workaround
EXT_SITMPUSW-135 RTC Test application failing intermittently RTC 11.00.00 No known workaround
EXT_EP-12277 AM62Px: ECC: SDL_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR aggregator is failing SDL 10.01.00 No known workaround
EXT_EP-12279 CSI RX ECC aggregators are failing on AM62P/AM62X SDL 09.01.00 No known workaround
EXT_EP-12280 Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F - After running MCU LBIST, not able to connect to any core through JTAG on AM62px SDL 09.00.00 No known workaround
EXT_EP-12276 ECC: Firewall related aggregators failures - ECC Aggregators SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR, SDL_SA3_SS0_SA3SS_AM62A_SA_UL_ECC_AGGR fail because of firewall access issues faced by SDL SDL 10.01.00 No known workaround

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader
3 The EVM is limited to only one MAC address in the EEPROM, applications requiring multiple MAC addresses should enable and configure manual MAC address entry in Sysconfig. Networking

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module

Migration guide

Older version

Newer version

Bootloader

Bootloader Migration Guidelines ‍

<= 10.01.00

>= 11.00.00

NETWORKING

Enet MCU+ SDK Update ‍

11.00.00

>= 11.01.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path `` in the file that uses `cb_lld_notify_linkchange`.