DDR
Attention
Please note that this driver is supported only on DM R5(WKUP R5) as part SBL examples. It is not supported on MCU-R5.
The DDR driver provides API to configure the DDR module.
Features Supported
Ability to enable/disable DDR support in your application
Ability to specify the DDR config generated using the “DDR SUBSYSTEM REGISTER CONFIGURATION” tool
Ability to enable/disable inline ECC (1b and 2b) in the application
Add regions for enabling inline ECC
SysConfig Features
Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
Ability to specify the DDR config generated using the “DDR SUBSYSTEM REGISTER CONFIGURATION” tool
Enables DDR, EMIF module clock when DDR module is selected
Toggle inline ECC functionality
Add regions for which inline ECC needs to be enabled
Ability to set the SDRAM index based on the connected DDR size
Features not Supported
NA
Creating your own DDR config file
Step 1: Generate a DDR config file for your EVM
Select “Software Product” as “DDR SUBSYSTEM REGISTER CONFIGURATION”
Select “Device” of interest, AM62PX in this case.
DDR SUBSYSTEM REGISTER CONFIGURATION Tool
Configure the DDR parameters using the tool
Save the generated
board_ddrReginit.hin your project workspace or work area
Configure and save the generated file
Step 2: Add the generated DDR config file to your project
Open SysConfig (Using SDK with SysConfig) for your project
Add “DDR” as shown below
Add DDR via SysConfig
Specify the path to the generated
board_ddrReginit.hfile including the filename in the sysconfig text box as shown aboveMake sure to use forward slash “/” in the file path so that this will work with linux as well as windows build
Make sure that path to this is file set in your application include path, as needed.
Save the sysconfig project and build your application
Creating your own LPDDR config file
Step 1: Generate a LPDDR config file for your EVM
Select “Software Product” as “DDR SUBSYSTEM REGISTER CONFIGURATION”
Select “Device” of interest, AM62PX in this case. The tool UI is the same as shown in Step 1: Generate a DDR config file for your EVM.
Configure the LPDDR parameters using the tool
Save the generated
board_ddrReginit.hin your project workspace or work area. Rename the file as “board_lpddrReginit.h”.
Configure and save the generated file
Step 2: Add the generated LPDDR config file to your project
Open SysConfig (Using SDK with SysConfig) for your project
Add “DDR” as shown below
Add LPDDR via SysConfig
Specify the path to the generated
board_lpddrReginit.hfile including the filename in the sysconfig text box as shown aboveMake sure to use forward slash “/” in the file path so that this will work with linux as well as windows build
Make sure that path to this is file set in your application include path, as needed.
Save the sysconfig project and build your application
Enabling DDR inline ECC
For SDRAM data integrity, the DDRSS bridge supports inline ECC on the data written to or read from the SDRAM. ECC is stored together with the data so that a dedicated SDRAM device for ECC is not required. The 8-bit single error correction double error detection (SECDED) ECC data is calculated over 64-bit data quanta.
For every 256-byte (AM62X) or 512-byte (AM62AX/AM62DX/AM62PX) data block, 32 or 64 bytes of ECC is stored inline respectively.
Thus 1/9th of the total SDRAM space is used for ECC storage and the rest 8/9th is available for system use. From system point of view that 8/9th of the SDRAM data space are seen as consecutive byte addresses. DDRSS supports up to 3 ECC protected non-overlapping memory ranges.
Attention
When inline ECC is enabled, the last 1/9th part of the DDR memory should not used. This rule applies irrespective of the size of the ECC regions.
Step 1: Enable inline ECC in the SBL sysconfig
Open the SBL SysConfig file and configure the inline ECC settings as described below.
Open SysConfig file (Using SDK with SysConfig) of your SBL
Calculate the SDRAM index based on your connected DDR size and update the field
Formula: SDRAM index = log2(connected DDR size) - 16
Enable inline ECC and add regions for which inline ECC needs to be enabled as shown.
Enable inline ECC via SysConfig
Things to take care when adding ECC regions,
The address (ECC start and end) has to be specified as an offset from the DDR region start
The ECC region is inclusive of the start and end address.
The ECC region start address and the size should be aligned to 0x10000 bytes
The ECC region size has to be in the powers of two and greater than 0x10000 bytes
ECC region size = ECC region end address - ECC region start address + 1
When ECC is enabled, BIST engine primes only the 8/9th portion of the given size. So the actual ECC end address will be lesser than the given ECC address.
For the given ECC region, the actual end address will be calculated and displayed in the sysconfig
When ECC is enabled, last 1/9th of the total SDRAM space is used for ECC storage and the rest 8/9th is available for system use.
So 8/9th of the given ECC region should not fall under the last 1/9th part of the DDR memory.
Sysconfig files will get generated only if all the above conditions are met, otherwise it will throw an error.
Note
If you are using older release and migrating to 09_02 SDK, please make sure the above conditions are met in the added ECC regions.
Save the sysconfig project.
In the SBL, before using the DDR memory check if DDR init is done using the DDR_isInitDone function.
while(!DDR_isInitDone()) { ClockP_usleep(100); }Build the SBL
Step 2: Generate linux appimage and u-boot.img
If SBL is booting linux, last 1/9th of the DDR memory should not used anywhere in the linux and it has to be reserved in the device tree for storing ECC values.
For u-boot flow:
Reduce the “DDR memory” to 8/9th of whole DDR size in u-boot device tree by modifying the device tree board file (arch/arm/dts/k3-am62p5-sk.dts)
Rebuild a53 spl and u-boot.img with this change. Instructions to build A53 uboot can be found in the SDK Linux documentation at Foundational Components » U-Boot » User’s Guide » General Information » Build U-Boot
Generate the linux.appimage using the updated A53 SPL
Refer Linux Appimage Generator Tool for more details
Flash the linux.appimage and u-boot.img
For Falcon mode (fast bootmode):
Reduce the “DDR memory” to 8/9th of whole DDR size in linux device tree by modifying the device tree board file (arch/arm64/boot/dts/ti/k3-am62p5-sk.dts)
Rebuild the linux devicetree blob (dtb). For more information, refer the Linux SDK docs, section Foundational Components > Kernel > Users Guide
Generate the linux.appimage using the updated dtb file
Refer Linux Appimage Generator Tool for more details
Flash the linux.appimage
Important Usage Guidelines
Follow these guidelines when configuring and using the DDR driver.
Ideally DDR should be enabled in the bootloader application and the SDK bootloader by default enables DDR by default.
Usage Overview
Include the below file to access the APIs
#include <stdio.h>
#include <drivers/ddr.h>
/* DDR register config .h file as generated from DDR SUBSYSTEM REGISTER CONFIGURATION tool
* Make sure path to this file is specified in your application project/makefile include path
*/
#include "drivers/ddr/v0/soc/am64x_am243x/board_ddrReginit.h"
static DDR_Params gDdrParams =
{
/* below values are set using the globals defined in drivers/ddr/v0/soc/am64x_am243x/board_ddrReginit.h */
.clk1Freq = DDRSS_PLL_FREQUENCY_1,
.clk2Freq = DDRSS_PLL_FREQUENCY_2,
.ddrssCtlReg = DDRSS_ctlReg,
.ddrssPhyIndepReg = DDRSS_phyIndepReg,
.ddrssPhyReg = DDRSS_phyReg,
.ddrssCtlRegNum = DDRSS_ctlRegNum,
.ddrssPhyIndepRegNum = DDRSS_phyIndepRegNum,
.ddrssPhyRegNum = DDRSS_phyRegNum,
.ddrssCtlRegCount = DDRSS_CTL_REG_INIT_COUNT,
.ddrssPhyIndepRegCount = DDRSS_PHY_INDEP_REG_INIT_COUNT,
.ddrssPhyRegCount = DDRSS_PHY_REG_INIT_COUNT,
.fshcount = DDRSS_PLL_FHS_CNT,
.enableEccFlag = 0,
.eccRegion = NULL,
};
Initialize DDR
DDR_init(&gDdrParams);
Example Usage
NA
API Reference
This file contains DDR APIs.
Functions
-
void DDR_Params_init(DDR_Params *prms)
Set default values to DDR_Params.
- Parameters:
prms – [out] Pointer to DDR configuration.
-
int32_t DDR_init(DDR_Params *prms)
DDR4 Initialization function.
Initializes the DDR timing parameters. Sets the DDR timing parameters based in the DDR PLL controller configuration. Any changes to DDR PLL requires change to DDR timing.
- Parameters:
prms – [in] Pointer to DDR configuration.
- Returns:
status SystemP_SUCCESS in case of success or appropriate error code
-
void DDR_enableInlineECC(uint8_t enableFlag)
Enable/Disable DDR inline ECC.
- Parameters:
enableFlag – [in] Flag to enable or disable DDR Inline ECC
-
int32_t DDR_clearECCError(uint8_t errorType)
Clear ECC errors for DDR.
- Parameters:
errorType – [in] DDR ECC error type (single bit/two bit ECC)
- Returns:
status SystemP_SUCCESS in case of success or appropriate error code
-
int32_t DDR_getECCErrorInfo(DDR_ECCErrorInfo *ECCErrorInfo)
Get ECC error status.
- Parameters:
ECCErrorInfo – [out] Get DDR ECC error bit status
- Returns:
status SystemP_SUCCESS in case of success or appropriate error code
-
uint8_t DDR_isInitDone(void)
Check if DDR init is done.
- Returns:
0 if DDR init is not completed else 1
-
struct DDR_EccRegion
- #include <ddr.h>
DDR Inline ECC region The structure specifies the DDR inline ECC region start and End address.
Public Members
-
uint64_t ddrEccStart0
DDR inline ECC region-0 start address
-
uint64_t ddrEccEnd0
DDR inline ECC region-0 end address
-
uint64_t ddrEccPrimeEnd0
DDR inline ECC region-0 primed end address
-
uint64_t ddrEccStart1
DDR inline ECC region-1 start address
-
uint64_t ddrEccEnd1
DDR inline ECC region-1 end address
-
uint64_t ddrEccPrimeEnd1
DDR inline ECC region-1 primed end address
-
uint64_t ddrEccStart2
DDR inline ECC region-2 start address
-
uint64_t ddrEccEnd2
DDR inline ECC region-2 end address
-
uint64_t ddrEccPrimeEnd2
DDR inline ECC region-2 primed end address
-
uint64_t ddrEccStart0
-
struct DDR_Params
- #include <ddr.h>
DDR config structure.
Below arrays and values are generated using the separate DDR config tool
ddrssCtlReg,ddrssPhyIndepReg,ddrssPhyRegddrssCtlRegNum,ddrssPhyIndepRegNum,ddrssPhyIndepRegNumddrssCtlRegCount,ddrssPhyIndepRegCount,ddrssPhyRegCount
Public Members
-
uint64_t clk1Freq
DDR Frequency of operation, in Hz
-
uint64_t clk2Freq
DDR Frequency of operation, in Hz
-
uint32_t *ddrssCtlReg
Array of register value to set
-
uint32_t *ddrssPhyIndepReg
Array of register value to set
-
uint32_t *ddrssPhyReg
Array of register value to set
-
uint16_t *ddrssCtlRegNum
Array of register numbers into which the values
ddrssCtlRegwill be set
-
uint16_t *ddrssPhyIndepRegNum
Array of register numbers into which the values
ddrssPhyIndepRegwill be set
-
uint16_t *ddrssPhyRegNum
Array of register numbers into which the values
ddrssPhyRegwill be set
-
uint16_t ddrssCtlRegCount
Number of elements in array
ddrssCtlReg
-
uint16_t ddrssPhyIndepRegCount
Number of elements in array
ddrssCtlReg
-
uint16_t ddrssPhyRegCount
Number of elements in array
ddrssCtlReg
-
uint8_t fshcount
Frequency Handshake count
-
uint8_t sdramIdx
log2(connected SDRAM size) - 16
-
uint8_t enableEccFlag
Flag to enable Inline ECC
-
DDR_EccRegion *eccRegion
Inline ECC region address
-
struct DDR_ECCErrorInfo
- #include <ddr.h>
Emif ECC Error Information structure.
This structure provides information about the ECC error