Release Notes 12.00.00

Attention

Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.

Note

The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination. Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC

Supported CPUs

EVM

Host PC

AM62P

MCU R5F, WKUP R5F

SK-AM62P-LP EVM (referred to as am62px-sk in code)

Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Note

Update of OSPI tuning algorithm on this SDK causes increase in tuning time. Refer OSPI NOR Flash Performance

Feature

Module

PADCFG drive strength adjustment through SYSCFG

Pinmux

LBIST/PBIST initiated in SBL EMMC

SBL

Enable WKUP-R5F ATCM

SBL

Watchdog support for DM R5/WKUP-R5F

WDT

Save/Restore of FPU registers on context switch enabled by default on A53

FreeRTOS

MMCSD drive strength as a configurable option

MMCSD

Add 8S-8S-8S protocol support

OSPI

Route SecProxy event for MCU cores

DM

Interrupt mode in SCIClient

SCI Client

Move task stack allocation to application layer

SCI Server

Add WFI in MCU only mode to save power

LPM

Experimental Features

Attention

  • Features listed below are early versions and should be considered as “experimental”.

  • Users can evaluate the feature, however the feature is not fully tested at TI side.

  • TI would not support these feature on public e2e.

  • Experimental features will be enabled with limited examples and SW modules.

Feature

Module

Ethernet traffic sharing accross multiple cores, called Ethernet Firmware

Networking

C++ SUpport

NA

Dependent Tools and Compiler Information

Attention

It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recommended and may cause TIFS/ DM functionality to break.

Tools/Components

Supported CPUs

Version

Code Composer Studio

MCU-R5F, WKUP-R5F

20.3.1

SysConfig

MCU-R5F, WKUP-R5F

1.24.2, build 4234

TI ARM CLANG

MCU-R5F, WKUP-R5F

4.0.1.LTS

GCC AARCH64

A53

9.2-2019.12

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

11.1.0

SDK Components

SYSFW / TIFS

Version 12.00.02
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS

Supported CPUs

SysConfig Support

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

NA

FreeRTOS POSIX

MCU-R5F

NA

No RTOS

MCU-R5F, WKUP-R5F

NA

Driver Porting Layer (DPL)

Module

Supported CPUs

SysConfig Support

OS support

Address Translate

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Cache

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Clock

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

CycleCounter

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Debug

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Heap

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Hwi

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

MPU

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Semaphore

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Task

MCU-R5F, WKUP-R5F

NA

FreeRTOS

Timer

MCU-R5F, WKUP-R5F

Yes

FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode

Supported CPUs

SysConfig Support

PHY Support

DMA Support

OS support

OSPI NOR

WKUP-R5F

Yes

Yes

Yes

NORTOS

EMMC

WKUP-R5F

Yes

NA

NA

NORTOS

UART

WKUP-R5F

Yes

NA

No

NORTOS

SDL

SDL Module

Supported CPUs

SysConfig Support

MCRC

MCU-R5F

No

ESM

MCU-R5F

No

VTM

MCU-R5F

No

DCC

MCU-R5F

No

ECC

MCU-R5F

No

RTI

MCU-R5F

No

POK

MCU-R5F

No

STOG

MCU-R5F

No

MTOG

MCU-R5F

No

PBIST

MCU-R5F

No

LBIST

MCU-R5F

No

ROM_CHECKSUM

MCU-R5F

No

Networking

Module

Supported CPUs

SysConfig Support

OS Support

Key features tested

Key features not tested

TSN

WKUP-R5F

NO

FreeRTOS

gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration

Multi-Clock Domain

LwIP

WKUP-R5F

YES

FreeRTOS

TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver

Other LwIP features

Ethernet driver (ENET)

WKUP-R5F

YES

FreeRTOS

Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, Strapped PHY (Early Ethernet), cut through switch on CPSW

RMII mode

SOC Device Drivers

Note

See the updated MCASP usage guidelines in MCASP for changes in MCASP driver

Peripheral Domain Supported CPUs SysConfig Support
DDR Main WKUP-R5F Yes
ECAP Main MCU-R5F Yes
EPWM Main MCU-R5F, WKUP-R5F Yes
DSS Main WKUP-R5F Yes
GPIO MCU MCU-R5F, WKUP-R5F Yes
Main MCU-R5F, WKUP-R5F Yes
I2C Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
IPC Main MCU-R5F, WKUP-R5F Yes
MCAN MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
MCASP Main WKUP-R5F Yes
MCSPI Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
MMCSD Main WKUP-R5F, MCU-R5F Yes
OSPI Main WKUP-R5F Yes
Pinmux Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup MCU-R5F, WKUP-R5F Yes
PMU Wakeup WKUP-R5F Yes
SOC NA MCU-R5F, WKUP-R5F Yes
SCIClient NA MCU-R5F, WKUP-R5F Yes
RTC MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
UART Main MCU-R5F, WKUP-R5F Yes
MCU MCU-R5F, WKUP-R5F Yes
Wakeup WKUP-R5F Yes
UDMA MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
WDT Wakeup WKUP-R5F Yes

Board Device Drivers

Peripheral

Supported CPUs

SysConfig Support

EEPROM

MCU-R5F, WKUP-R5F

Yes

Ethernet PHY

WKUP-R5F

Yes

Flash

WKUP-R5F

Yes

LED

MCU-R5F, WKUP-R5F

Yes

PMIC

MCU-R5F

Yes

Fixed Issues

ID Head Line Module
EXT_SITMPUSW-245 MCU+ SDK LPDDR4 Driver starts DDR Training/Leveling Sequence twice DDR
EXT_SITMPUSW-293 Sciclient driver uses incorrect context for the TISCI_MSG_KEYRING_IMPORT DM
EXT_SITMPUSW-309 LPM: Spurious wake up on MCU only mode DM
EXT_SITMPUSW-312 Incorrect context description of SCICLIENT_CONTEXT_DM2TIFS DM
EXT_SITMPUSW-288 LPM: Unable to enter LPM in Interrupt Mode DM
EXT_SITMPUSW-302 Compilation Errors when disabling DebugP logs. DPL
EXT_SITMPUSW-251 MCU+ SDK Example Projects using incorrect ARMv7 MPU Attributes for Peripheral Register Region Examples
EXT_SITMPUSW-301 OSPI_norFlashInit1s1s1s has an implementation of wait for 500 milliseconds instead of microseconds Flash
EXT_SITMPUSW-282 Sysconfig not generating code for GPIO Trigger GPIO
EXT_SITMPUSW-279 I2C close is not working properly during error conditions I2C
EXT_SITMPUSW-310 Incorrect handling of the timeout for the CMD6 command MMCSD
EXT_SITMPUSW-114 MMCSD_enableBootPartition implements two mutually exclusive concepts as one function MMCSD
EXT_SITMPUSW-295 Flash Close Logic Requires OSPI Handle to be reset to 1S-1S-1S OSPI
EXT_SITMPUSW-280 OSPI Indac Mode Should Check for odd bytes OSPI
EXT_SITMPUSW-256 Incorrect calculation of rowColEnd in the ext_otp_writeMmr OTP
EXT_SITMPUSW-292 Bootloader_socOpenFirewalls is called before System_init in the SBLs SBL
EXT_SITMPUSW-214 WDT: Hang due to no valid argument check in APIs Watchdog
EXT_EP-13267 SDL ESM: Wrong instance argument in SDL_ESM_loInterruptHandler causing misidentification of ESM0 interrupts SDL-ESM

Known Issues

ID Head Line Module
EXT_SITMPUSW-153 MCU+ SDK CCS Project Build Generates Invalid/Redundant Boot Image Files Build
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC
EXT_SITMPUSW-259 eMMC retuning may be attempted during the initialization sequence MMCSD
EXT_SITMPUSW-222 MMCSD field Card Type is not ordered logically in the Sysconfig MMCSD
EXT_SITMPUSW-135 RTC Test application failing intermittently. RTC
EXT_SITMPUSW-220 SBL_SD bootloaders report incorrect boot image size SBL
EXT_SITMPUSW-324 UART_udmaIsrTx does not handles continuous Callbacks properly UART
EXT_SITMPUSW-258 WKUP UART0 is not working in CallBack mode UART
EXT_EP-12276 ECC: Firewall related aggregators failures SDL-ECC
EXT_EP-12277 AM62Px: ECC: SDL_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR aggregator is failing SDL-ECC
EXT_EP-12279 CSI RX ECC aggregators are failing on AM62P/AM62X SDL-ECC
EXT_EP-13265 MCU R5 ECC Aggr init fails when MCU LBIST is enabled in bootloader SDL-LBIST
EXT_EP-12280 Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F SDL-LBIST

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 LPM is not supported with SBL boot flow. It is supported only with SPL boot flow. Bootloader
3 The EVM is limited to only one MAC address in the EEPROM, applications requiring multiple MAC addresses should enable and configure manual MAC address entry in Sysconfig. Networking

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module

Migration guide

Older version

Newer version

Bootloader

Bootloader Migration Guidelines ‍

<= 10.01.00

>= 11.00.00

NETWORKING

Version Updates from earlier SDKs to Latest ‍

<= 11.01.00

>= 11.02.00

OSPI

OSPI Migration Guide ‍

<= 11.01.00

>= 11.02.00

SCI Server

Migration Guide 11.02 to 12.00 ‍

<= 11.02.00

>= 12.00.00

SBL Linker

Migration Guide 11.02 to 12.00 ‍

<= 11.02.00

>= 12.00.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path `` in the file that uses `cb_lld_notify_linkchange`.