OTP Revision Example
Introduction
This example demonstrates how to get the software revision, key revision, key count and update the software revision runtime. For now, only the software revision update for secure boardcfg is supported. In a fresh sample, the revision number would be 1U. Example reads the SWREV revision first. If the revision number is 0U, then it tries to write 1U to the eFUSE. The SWREV value written to the eFUSE can be changed based on the requirement. This example is supported only in HS-SE devices. This is a special example, and is booted by ROM. Because of this it is to be treated like a bootloader application. It makes use of Sciclient API calls to do this, there are wrapper functions provided in the example for this.
Supported Combinations
Parameter |
Value |
|---|---|
CPU + OS |
wkup-r5fss0-0 nortos |
Toolchain |
ti-arm-clang |
Board |
am62px-sk |
Example folder |
examples/otp/otp_revision/ |
Steps to Run the Example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
Set bootmode to UART and flash the binary using the following command from {SDK_INSTALLTION_PATH}/tools/boot
python uart_uniflash.py -p /dev/ttyUSB0 --cfg=../../examples/otp/otp_revision/am62px-sk/wkup-r5fss0-0_nortos/default_otp_revision_hs.cfg
Power OFF and change the boot mode to OSPI NOR BOOT MODE
Logs should appear at the WKUP_UART0
Sample Output
Shown below is a sample output when the application is run:
Starting Runtime OTP revision writer
SWREV read : 0x1
SWREV already written to eFUSE, value : 0x1
Value of Key REV: 0x1 and key count: 0x1
All tests have passed!!