Runtime debug unlock Example

Introduction

In HS-SE device, the JTAG debug port is closed by default. The user can do runtime debug unlock by sending a TISCI message with a signed debug certificate. This example demonstrates how to do runtime JTAG port unlock. If the JTAG is unlocked, the example passes. The example is supported only on HS-SE device.

Refer TISCI documentation for more details about the API.

Note

Only hosts allowed in security board configuration can send jtag unlock message via TISCI. Before running the example change the “allow_jtag_unlock”, “allow_wildcard_unlock” and “jtag_unlock_hosts” parameters in the “source/drivers/sciclient/sciclient_default_boardcfg/am62px/sciclient_defaultBoardcfg_security.c” as follows,

          .allow_jtag_unlock = 0x5A,
       .allow_wildcard_unlock = 0x5A,
       .jtag_unlock_hosts = {TISCI_HOST_ID_WKUP_0_R5_0, 0, 0, 0},

Supported Combinations

Parameter

Value

CPU + OS

wkup-r5fss0-0 freertos

Toolchain

ti-arm-clang

Boards

am62px-sk

Example folder

examples/security/runtime_debug_unlock

Steps to Run the Example

Generate debug certificate

Build the example

Sample Output

Shown below is a sample output when the application is run,

Runtime debug unlock example!
Run time JTAG debug unlock... DONE !!!
All tests have passed!!