Timer
Features Supported
APIs to setup timer configuration
APIs to start and stop the timer
APIs to get the current timer count
APIs to check for counter overflow and clear timer overflow interrupt
Features NOT Supported
NA
Important Usage Guidelines
Supports continues and oneshot mode
When configuring the timer period in micro second the ‘periodInNsec’ should be set to 0
Example Usage
Include the below file to access the APIs,
//! [include]
#include <kernel/dpl/TimerP.h>
//! [include]
void samples(uint32_t timerBaseAddr)
{
{
//! [initialize]
TimerP_Params timerParams;
Example usage to initialize the timer:
TimerP_Params_init(&timerParams);
timerParams.inputPreScaler = 1u;
timerParams.inputClkHz = 250u*1000u*1000u;
timerParams.periodInUsec = 10u*1000u;
timerParams.oneshotMode = 0;
timerParams.enableOverflowInt = 1;
TimerP_setup(timerBaseAddr, &timerParams);
//! [initialize]
}
{
//! [start]
/* start the tick timer */
TimerP_start(timerBaseAddr);
//! [start]
}
{
//! [curCount]
uint32_t count;
/* start the tick timer */
count = TimerP_getCount(timerBaseAddr);
(void) count; /* kill warning of variable set but not used */
//! [curCount]
}
{
//! [stop]
/* stop the tick timer */
TimerP_stop(timerBaseAddr);
//! [stop]
Example usage to start the timer:
}
{
//! [start]
/* start the tick timer */
TimerP_start(timerBaseAddr);
//! [start]
Example usage to get the current count value:
//! [curCount]
uint32_t count;
/* start the tick timer */
count = TimerP_getCount(timerBaseAddr);
(void) count; /* kill warning of variable set but not used */
//! [curCount]
Example usage to stop the timer:
//! [stop]
/* stop the tick timer */
TimerP_stop(timerBaseAddr);
//! [stop]
API Reference
Defines
-
TIME_IN_MICRO_SECONDS
Macro defines the time in micro seconds
-
MAX_TIMER_COUNT_VALUE
Macro defines the maximum timer count value
-
TIME_IN_MILLI_SECONDS
Macro defines the time in milli seconds
-
TIME_IN_NANO_SECONDS
Macro defines the time in nano seconds
-
TIMERP_SHIFT_BY_EIGHT
Macro defines the shift by eight
-
MAX_NUMBER_OF_CYCLES
Macro defines the maximum number of cycles
Functions
-
void TimerP_Params_init(TimerP_Params *params)
Set default value for TimerP_Params.
- Parameters:
params – [out] timer parameters initalized to default
-
int32_t TimerP_setup(uint32_t baseAddr, TimerP_Params *params)
Setup timer but does not start it.
- Parameters:
baseAddr – [in] HW timer base addresss
params – [in] timer parameters
- Returns:
SystemP_SUCCESS on success, SystemP_FAILURE if baseAddr is 0, params is NULL, or any parameter value is invalid
-
int32_t TimerP_start(uint32_t baseAddr)
Start timer.
- Parameters:
baseAddr – [in] HW timer base addresss
-
int32_t TimerP_stop(uint32_t baseAddr)
Stop timer.
- Parameters:
baseAddr – [in] HW timer base addresss
-
uint32_t TimerP_getCount(uint32_t baseAddr)
Get timer current count.
- Parameters:
baseAddr – [in] HW timer base addresss
- Returns:
current timer count value
-
uint32_t TimerP_getReloadCount(uint32_t baseAddr)
Get timer reload count.
- Parameters:
baseAddr – [in] HW timer base addresss
- Returns:
reload count value
-
int32_t TimerP_clearOverflowInt(uint32_t baseAddr)
Clear timer overflow interrupt.
- Parameters:
baseAddr – [in] HW timer base addresss
-
uint32_t TimerP_isOverflowed(uint32_t baseAddr)
Check if timer is overflowed.
Note
make sure to clear overflow status TimerP_clearOverflowInt
- Parameters:
baseAddr – [in] HW timer base addresss
-
struct TimerP_Params
- #include <TimerP.h>
Parameters for TimerP_setup.
Public Members
-
uint32_t inputPreScaler
input pre-scaler divisor ro apply
Note
MUST be power of 2 and between 1 and 256 for GP Timer
Note
MAKE sure this value is not 0
Note
This field is valid only when underlying timer is DM Timer.
Note
This field is not valid when underlying timer is RTI Timer. Set to 1 in this case.
-
uint32_t inputClkHz
Timer input clock in unit of Hz before pre-scaler, system initialization MUST make any system level muxes, PLLs, power required to input this clock are setup properly
Note
MAKE sure this value is not 0
-
uint32_t periodInUsec
Timer period in units of usecs, internally TimerP_Params::inputClkHz and TimerP_Params.inputPreScaler is used to compute the value to be put inside the timer HW register
Note
When value is 0, periodInNsec is used instead
Note
When both periodInUsec and periodInNsec are non-zero, periodInNsec is used
-
uint64_t periodInNsec
Timer period in units of nsecs, internally TimerP_Params::inputClkHz and TimerP_Params.inputPreScaler is used to compute the value to be put inside the timer HW register
Note
When value is 0, periodInUsec is used instead
Note
When both periodInUsec and periodInNsec are non-zero, periodInNsec is used
-
uint32_t oneshotMode
0: continuous mode of operation, 1: oneshot mode of operation
Note
NOT supported for RTI timer, always set to 0 in this case.
-
uint32_t enableOverflowInt
0: Do not enable timer overflow interrupt, 1: enable timer overflow interrupt
-
uint32_t enableDmaTrigger
0: Do not enable DMA trigger from timer, 1: enable DMA trigger from timer
-
uint32_t inputPreScaler