RTI
The Windowed Watchdog Timer (WWDT) generates reset after a programmable period, if not serviced within that period. This time-out boundary is configurable, and the windowed feature allows the start time boundary to be configurable. The WWDT can generate an Interrupt, if not serviced within window (Open Window) defined by start time and time-out boundary. Also the WWDT can generate an Interrupt if serviced outside Open Window (within Closed Window). Generation of Interrupt depends on the WWDT Reaction configuration. SDL supports configuration of the watchdog timers. It also supports notification of the error via ESM interrupt. Additionally, APIs for checking the status of the watchdog timer is provided.
Features Supported
The module provides the following functionality
Ability to to initialize the RTI -DWWD module
Ability to configure RTI -DWWD module
Ability to service an RTI instance
Ability to read Status of the configuration
Ability to read back static register
There are 7 RTI Modules in the device – 1 in the MCU domain and 5 in the Main domain and 1 in wkup domain.
Instances in MCU domain:
MCU_RTI0
Instances in Main domain:
RTI0
RTI1
RTI2
RTI3
RTI15
Instances in WKUP domain:
WKUP_RTI0
SysConfig Features
None
Features NOT Supported
None
Important Usage Guidelines
None
Example Usage
The following shows an example of SDL RTI API.
Include the below file to access the APIs
#include <sdl/sdl_rti.h>
API Reference
Functions
-
int32_t SDL_RTI_config(SDL_RTI_InstanceType InstanceType, const SDL_RTI_configParms *pConfig)
RTI configuration API. This API configures the specified RTI instance using the provided configuration.
- Parameters:
InstanceType – RTI Instance
pConfig – Pointer to the configuration structure
- Returns:
SDL_PASS for Success. SDL Error Code for failure.
-
int32_t SDL_RTI_verifyConfig(SDL_RTI_InstanceType InstanceType, SDL_RTI_configParms *pConfig)
RTI API to verify the written configuration. This API can be used after calling SDL_RTI_config in order to verify the configuration. It reads back the configuration from the registers and compares it with the provided configuration.
- Parameters:
InstanceType – RTI Instance
pConfig – Pointer to the configuration structure
- Returns:
SDL_PASS if verification passed. SDL Error Code for failure.
-
int32_t SDL_RTI_start(SDL_RTI_InstanceType InstanceType)
Enable the RTI instance.
Note
Should be called after configuration of the RTI
- Parameters:
InstanceType – RTI Instance
- Returns:
SDL_PASS if success. SDL Error Code for failure.
-
int32_t SDL_RTI_service(SDL_RTI_InstanceType InstanceType)
Service the RTI instance.
- Parameters:
InstanceType – RTI Instance
- Returns:
SDL_PASS if success. SDL Error Code for failure.
-
int32_t SDL_RTI_clearStatus(SDL_RTI_InstanceType InstanceType, uint32_t status)
Clear the DWWD status.
- Parameters:
InstanceType – RTI Instance
status – Violation status to clear. Values given by bitwise or of macro RTI_Status_t
- Returns:
SDL_PASS if success. SDL Error Code for failure.
-
int32_t SDL_RTI_getStatus(SDL_RTI_InstanceType InstanceType, uint32_t *pStatus)
Clear the DWWD status.
- Parameters:
InstanceType – RTI Instance
pStatus – pointer to DWWD status. Refer macro RTI_Status_t for possible bitwise or of all return values.
- Returns:
SDL_PASS if success. SDL Error Code for failure.
-
int32_t SDL_RTI_readStaticRegs(SDL_RTI_InstanceType InstanceType, SDL_RTI_staticRegs *pStaticRegs)
This API returns the static registers for RTI-DWWD.
- Parameters:
InstanceType – Base Address of the RTI instance.
pStaticRegs – Pointer to RTI DWWD Static Registers.
- Returns:
SDL_PASS if success. SDL Error Code for failure.