Release Notes 09.01.00

Attention

Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.

Note

The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination. Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC

Supported CPUs

EVM

Host PC

AM62P

MCU R5F, WKUP R5F

SK-AM62P-LP EVM (referred to as am62px-sk in code)

Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Feature

Module

FreeRTOS support on MCU R5F and WKUP R5F

OS

UART, SCI Client, IPC, GPIO, I2C, MCAN and MCSPI drivers on MCU R5F

Drviers

UART, SCI Client, IPC, GPIO, I2C, MCAN, MCSPI, DDR, OSPI, EMMC and DM on WKUP R5F

Drviers

DSS support on WKUP R5F

Drviers

McASP suport on WKUP R5F

Drviers

DSS freeze frame detect, data integrity check

DSS

MCU domain reset isolation, firewall isolation

Safety

Dependent Tools and Compiler Information

Tools

Supported CPUs

Version

Code Composer Studio

MCU-R5F, WKUP-R5F

12.5.0

SysConfig

MCU-R5F, WKUP-R5F

1.18.0, build 3266

TI ARM CLANG

MCU-R5F, WKUP-R5F

3.2.0.LTS

GCC AARCH64

A53

9.2-2019.12

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

10.6.1

Key Features

OS Kernel

OS

Supported CPUs

SysConfig Support

FreeRTOS Kernel

MCU-R5F, WKUP-R5F

NA

FreeRTOS POSIX

MCU-R5F

NA

NO RTOS

MCU-R5F, WKUP-R5F

NA

Driver Porting Layer (DPL)

Module

Supported CPUs

SysConfig Support

OS support

Address Translate

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

Cache

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

Clock

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

CycleCounter

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Debug

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

Heap

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Hwi

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

MPU

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

Semaphore

MCU-R5F, WKUP-R5F

NA

FreeRTOS, NORTOS

Task

MCU-R5F, WKUP-R5F

NA

FreeRTOS

Timer

MCU-R5F, WKUP-R5F

YES

FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode

Supported CPUs

SysConfig Support

PHY Support

DMA Support

OS support

OSPI NOR

WKUP-R5F

YES

YES

YES

NORTOS

EMMC

WKUP-R5F

YES

NA

NA

NORTOS

UART

WKUP-R5F

YES

NA

No

NORTOS

SDL

SDL Module

Supported CPUs

SysConfig Support

MCRC

MCU-R5F

NO

ESM

MCU-R5F

NO

VTM

MCU-R5F

NO

DCC

MCU-R5F

NO

ECC

MCU-R5F

NO

RTI

MCU-R5F

NO

POK

MCU-R5F

NO

STOG

MCU-R5F

NO

MTOG

MCU-R5F

NO

POK

MCU-R5F

NO

PBIST

MCU-R5F

NO

LBIST

MCU-R5F

NO

ROM_CHECKSUM

MCU-R5F

NO

Note

This is EA(early adopter) version for SDL. GA(General Availability) release will be provided in next release.

SOC Device Drivers

Peripheral Domain Supported CPUs SysConfig Support
DDR Main WKUP-R5F YES
DSS Main WKUP-R5F YES
GPIO MCU MCU-R5F, WKUP-R5F YES
Main MCU-R5F, WKUP-R5F YES
I2C Main MCU-R5F, WKUP-R5F YES
MCU MCU-R5F, WKUP-R5F YES
Wakeup MCU-R5F, WKUP-R5F YES
IPC Main MCU-R5F, WKUP-R5F YES
MCAN MCU MCU-R5F YES
MCASP Main WKUP-R5F YES
MCSPI Main MCU-R5F, WKUP-R5F YES
MCU MCU-R5F, WKUP-R5F YES
Pinmux Main MCU-R5F, WKUP-R5F YES
MCU MCU-R5F, WKUP-R5F YES
Wakeup MCU-R5F, WKUP-R5F YES
SOC NA MCU-R5F, WKUP-R5F YES
SCIClient NA MCU-R5F, WKUP-R5F YES
UART Main MCU-R5F, WKUP-R5F YES
MCU MCU-R5F, WKUP-R5F YES
Wakeup WKUP-R5F YES

Fixed Issues

NA

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-208 gmake with -j can sometimes lock up Windows command prompt Build 9.0.1 Use bash for windows as part of git for windows or don't use -j option
PROC_SDL-7044 ECC is not supported for some instances. These are SDL_DSS_DSI0_K3_DSS_DSI_DSI_TOP_ECC_AGGR_SYS SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR SDL 9.1.0 None. Support will be added in future release.
PROC_SDL-7045 ESM example is failing. SDL 9.1.0 None. Support will be added in future release. ESM itself is working when it's integrated in to other SDL components.

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA