![]() |
![]() |
|
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
| CADC_Config_ | ADC Global configuration |
| CADC_FxnTable_ | The definition of a ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params_ | ADC Parameters |
| CADCBuf_Config_ | ADCBuf Global configuration |
| CADCBuf_Conversion_ | An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK |
| CADCBuf_FxnTable_ | The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation |
| CADCBuf_Params_ | ADC Parameters |
| CADCBufCC26XX_AdcChannelLutEntry | Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal |
| CADCBufCC26XX_HWAttrs | ADCBufCC26XX Hardware Attributes |
| CADCBufCC26XX_Object | ADCBufCC26XX Object |
| CADCBufCC26XX_ParamsExtension | CC26XX specfic extension to ADCBuf_Params |
| CADCCC26XX_HWAttrs | ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions |
| CADCCC26XX_Object | ADCCC26XX Object |
| CCamera_Config_ | Camera Global configuration |
| CCamera_FxnTable_ | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
| CCamera_Params_ | Camera Parameters |
| CCapture_Config_ | |
| CCapture_FxnTable_ | The definition of a Capture function table that contains the required set of functions to control a specific Capture driver implementation |
| CCapture_Params_ | Capture Parameters |
| CCryptoCC26XX_AESCBC_Transaction | CryptoCC26XX AES-CBC Transaction |
| CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
| CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
| CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
| CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
| CCryptoCC26XX_Object | CryptoCC26XX Object |
| CCryptoCC26XX_Params | CryptoCC26XX Parameters |
| CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayDogm1286_HWAttrs | |
| CDisplayDogm1286_Object | |
| CDisplayGrLib_Object | |
| CDisplayHost_HWAttrs | |
| CDisplayHost_Object | |
| CDisplaySharp_HWAttrs | |
| CDisplaySharp_Object | |
| CDisplaySharpColor_t | Foreground and background color struct, compatible with GrLib |
| CDisplayUart_HWAttrs | |
| CDisplayUart_Object | |
| CExtFlashInfo_t | |
| CGPIOCC26XX_Config | GPIO device specific driver configuration structure |
| CGPTimerCC26XX_Config | GPTimer Global configuration |
| CGPTimerCC26XX_HWAttrs | GPTimer26XX Hardware attributes |
| CGPTimerCC26XX_Object | GPTimer26XX Object |
| CGPTimerCC26XX_Params | GPTimerCC26XX Parameters |
| CI2C_Config_ | I2C global configuration |
| CI2C_FxnTable_ | The definition of an I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params_ | I2C Parameters |
| CI2C_Transaction_ | I2C transaction |
| CI2CCC26XX_HWAttrsV1 | I2CCC26XX Hardware attributes |
| CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
| CI2CSlave_Config_ | I2CSlave Global configuration |
| CI2CSlave_FxnTable_ | The definition of a I2CSlave function table that contains the required set of functions to control a specific I2CSlave driver implementation |
| CI2CSlave_Params_ | I2CSlave Parameters |
| CI2S_BufDesc_ | I2S buffer descriptor for issue/reclaim mode |
| CI2S_Config_ | I2S Global configuration |
| CI2S_FxnTable_ | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
| CI2S_Params_ | Basic I2S Parameters |
| CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
| CLCD_Command | Format of LCD commands used by the LCD controller |
| CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
| CLCD_HWAttrs | LCD Hardware attributes |
| CLCD_Object | LCD Object |
| CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
| CList_Elem | |
| CList_List | |
| CNVS_Attrs | NVS attributes |
| CNVS_Config | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CNVSCC26XX_CmdSetCopyBlockArgs | NVSCC26XX command structure for setting copy block |
| CNVSCC26XX_HWAttrs | NVSCC26XX attributes |
| CNVSCC26XX_Object | |
| CPDMCC26XX_BufferRequest | A PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer() |
| CPDMCC26XX_Config | The PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation |
| CPDMCC26XX_HWAttrs | PDMCC26XX Hardware attributes |
| CPDMCC26XX_I2S_AudioClockConfig | PDMCC26XX_I2S Audio Clock configuration |
| CPDMCC26XX_I2S_AudioFormatConfig | PDMCC26XX_I2S Hardware configuration |
| CPDMCC26XX_I2S_AudioPinConfig | PDMCC26XX_I2S Audio Pin configuration |
| CPDMCC26XX_I2S_BufferRelease | A PDMCC26XX_I2S_BufferRelease data structure is used with PDMCC26XX_I2S_releaseBuffer() |
| CPDMCC26XX_I2S_BufferRequest | A PDMCC26XX_I2S_BufferRequest data structure is used with PDMCC26XX_I2S_requestBuffer() |
| CPDMCC26XX_I2S_Config | The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation |
| CPDMCC26XX_I2S_HWAttrs | PDMCC26XX_I2S Hardware attributes |
| CPDMCC26XX_I2S_Object | PDMCC26XX_I2S Object |
| CPDMCC26XX_I2S_Params | PDMCC26XX I2S Parameters are used when calling PDMCC26XX_I2S_open() |
| CPDMCC26XX_I2S_StreamNotification | A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors |
| CPDMCC26XX_metaData | Metadata associated with an array of PCM data |
| CPDMCC26XX_Object | PDMCC26XX Object |
| CPDMCC26XX_Params | PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init() |
| CPDMCC26XX_pcmBuffer | PCM buffer pointed to in a PDMCC26XX_BufferRequest |
| CPDMCC26XX_StreamNotification | A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors |
| CPIN_State_s | Underlying data structure for type PIN_State |
| CPINCC26XX_HWAttrs | PINCC26XX Hardware attributes |
| CPower_NotifyObj_ | Power notify object structure |
| CPowerCC26XX_Config | Global configuration structure |
| CPowerCC26XX_ModuleState | PowerCC26XX_ModuleState |
| CPWM_Config_ | PWM Global configuration |
| CPWM_FxnTable_ | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params_ | PWM Parameters |
| CPWMTimerCC26XX_HwAttrs | PWMTimer26XX Hardware attributes |
| CPWMTimerCC26XX_Object | PWMTimer26XX Object |
| CRF_AccessParams | RF request access parameter struct RF request access command parameters are used with the RF_requestAccess() call |
| CRF_InfoVal | RF_getParamsVal used to input and return RF driver paramters with RF_getParams() |
| CRF_Mode | Struct defining operating mode of RF driver |
| CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
| CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
| CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
| CRF_ScheduleCmdParams | RF schedule command parameter struct RF schedule command parameters are used with the RF_scheduleCmd() call |
| CRF_ScheduleMap | RF schedule map structure |
| CRF_ScheduleMapElement | RF schedule map entry structure |
| CRFCC26XX_HWAttrs | RF Hardware attributes |
| CRingBuf_Object | |
| CSD_Config_ | SD Global configuration |
| CSD_FxnTable_ | The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation |
| CSD_Params_ | SD Parameters |
| CSDFatFS_Config_ | SDFatFS Global configuration |
| CSDFatFS_Object_ | SDFatFS Object The application must not access any member variables of this structure! |
| CSDSPI_Config_ | SDSPI Global configuration |
| CSDSPI_FxnTable_ | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
| CSDSPI_Params_ | SDSPI Parameters |
| CSPI_Config_ | SPI Global configuration |
| CSPI_FxnTable_ | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params_ | SPI Parameters |
| CSPI_Transaction_ | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| CSPICC26XXDMA_HWAttrsV1 | SPICC26XXDMA Hardware attributes |
| CSPICC26XXDMA_Object | SPICC26XXDMA Object |
| CTimer_Config_ | |
| CTimer_FxnTable_ | The definition of a Timer function table that contains the required set of functions to control a specific Timer driver implementation |
| CTimer_Params_ | Timer Parameters |
| CUART_Config_ | UART Global configuration |
| CUART_FxnTable_ | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params_ | UART Parameters |
| CUARTCC26XX_HWAttrsV2 | UARTCC26XX Hardware attributes |
| CUARTCC26XX_Object | UARTCC26XX Object |
| CUDMACC26XX_Config | UDMACC26XX Global configuration |
| CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
| CUDMACC26XX_Object | UDMACC26XX object |
| CWatchdog_Config_ | Watchdog Global configuration |
| CWatchdog_FxnTable_ | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params_ | Watchdog Parameters |
| CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
| CWatchdogCC26XX_Object | Watchdog Object for CC26XX |