![]() |
![]() |
|
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
| ADC.h | ADC driver interface |
| ADCBuf.h | ADCBuf driver interface |
| ADCBufCC26XX.h | ADCBuf driver implementation for a CC26XX analog-to-digital converter |
| ADCCC26XX.h | ADC driver implementation for the ADC peripheral on CC26XX |
| AnsiColor.h | |
| buzzer.h | PWM-based buzzer interface |
| Camera.h | Camera driver interface |
| Capture.h | Capture driver interface |
| Codec1.h | Implementation of TI Codec Type 1 (IMA ADPCM) encoding and decoding |
| CryptoCC26XX.h | Crypto driver implementation for a CC26XX Crypto controller |
| Display.h | Generic interface for text output |
| DisplayDogm1286.h | |
| DisplayExt.h | Extention of Display to access GrLib functionality in capable displays |
| DisplayHost.h | |
| DisplaySharp.h | |
| DisplayUart.h | Display.h implementation for UART output |
| ExtFlash.h | External flash storage abstraction |
| GPIO.h | GPIO driver |
| GPIOCC26XX.h | GPIO driver implementation for CC26xx/CC13xx devices |
| GPTimerCC26XX.h | GPTimer driver implementation for CC26XX/CC13XX |
| I2C.h | I2C driver interface |
| I2CCC26XX.h | I2C driver implementation for a CC26XX I2C controller |
| I2CSlave.h | I2CSlave driver interface |
| I2S.h | I2S driver interface |
| LCDDogm1286.h | LCD driver implementation for a DOGM128W-6 LCD display |
| LCDDogm1286_util.h | |
| List.h | Linked List interface for use in drivers |
| NVS.h | PRELIMINARY Non-Volatile Storage Driver |
| NVSCC26XX.h | |
| PDMCC26XX.h | PDM driver implementation for a CC26XX PDM controller |
| PDMCC26XX_util.h | PDM utility includes helper functions for configuring the CC26XX I2S controller |
| PIN.h | Generic PIN & GPIO driver |
| PINCC26XX.h | Device-specific pin & GPIO driver for CC26xx family [def] |
| Power.h | Power manager interface |
| PowerCC26XX.h | Power manager interface for CC26XX/CC13XX |
| PWM.h | PWM driver interface |
| PWMTimerCC26XX.h | PWM driver implementation for CC26XX/CC13XX |
| RF.h | RF driver for the CC26/13xx family |
| RingBuf.h | |
| SD.h | SD driver interface |
| SDFatFS.h | FATFS driver interface |
| SDSPI.h | SDSPI driver interface |
| SensorBmp280.h | Driver for the Bosch BMP280 Pressure Sensor |
| SensorHdc1000.h | Driver for Texas Instruments HCD1000 humidity sensor |
| SensorI2C.h | Simple interface to the TI-RTOS driver. Also manages switching between I2C-buses |
| SensorMpu9250.h | Driver for the InvenSense MPU9250 Motion Processing Unit |
| SensorOpt3001.h | Driver for the Texas Instruments OPT3001 Optical Sensor |
| SensorTagTest.h | Test code for SensorTag |
| SensorTmp007.h | Driver for the Texas Instruments TMP007 infra-red thermopile sensor |
| SensorUtil.h | Common utility code for SensorTag |
| SharpGrLib.h | |
| SPI.h | SPI driver interface |
| SPICC26XXDMA.h | SPI driver implementation for a CC26XX SPI controller using the UDMA controller |
| Timer.h | Timer driver interface |
| UART.h | UART driver interface |
| UARTCC26XX.h | UART driver implementation for a CC26XX UART controller |
| UDMACC26XX.h | UDMACC26XX driver implementation |
| Watchdog.h | Watchdog driver interface |
| WatchdogCC26XX.h | Watchdog driver implementation for CC13XX/CC26XX |