49 #ifndef ti_drivers_adc_ADCCC26XX__include
50 #define ti_drivers_adc_ADCCC26XX__include
66 #undef DEVICE_FAMILY_PATH
67 #define DEVICE_FAMILY_PATH(x) <ti/devices/DEVICE_FAMILY/x>
69 #error "You must define DEVICE_FAMILY at the project level as one of cc26x0, cc26x0r2, cc13x0, etc."
72 #include DEVICE_FAMILY_PATH(driverlib/aux_adc.h)
ADCCC26XX_Trigger_Source triggerSource
Definition: ADCCC26XX.h:149
Definition: ADCCC26XX.h:96
Definition: ADCCC26XX.h:89
ADCCC26XX_Reference_Source refSource
Definition: ADCCC26XX.h:147
ADCCC26XX Object.
Definition: ADCCC26XX.h:158
Definition: ADCCC26XX.h:120
bool isProtected
Definition: ADCCC26XX.h:162
Power manager interface for CC26XX/CC13XX.
struct ADCCC26XX_Object ADCCC26XX_Object
ADCCC26XX Object.
ADCCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCCC26XX.h:83
const ADC_FxnTable ADCCC26XX_fxnTable
ADCCC26XX_Trigger_Source
List of sources the ADC can be configured to trigger off of.
Definition: ADCCC26XX.h:130
Definition: ADCCC26XX.h:95
Device-specific pin & GPIO driver for CC26xx family [def].
Definition: ADCCC26XX.h:90
Definition: ADCCC26XX.h:93
Definition: ADCCC26XX.h:94
The definition of a ADC function table that contains the required set of functions to control a speci...
Definition: ADC.h:266
uint8_t adcCompBInput
Definition: ADCCC26XX.h:145
Definition: ADCCC26XX.h:85
underlying data structure for type PIN_State
Definition: PIN.h:687
uint8_t adcDIO
Definition: ADCCC26XX.h:144
bool isOpen
Definition: ADCCC26XX.h:161
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
Definition: ADCCC26XX.h:143
Definition: ADCCC26XX.h:88
Definition: ADCCC26XX.h:84
struct ADCCC26XX_HWAttrs ADCCC26XX_HWAttrs
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
PIN_Handle pinHandle
Definition: ADCCC26XX.h:160
PIN_State pinState
Definition: ADCCC26XX.h:159
Definition: ADCCC26XX.h:91
Definition: ADCCC26XX.h:86
bool inputScalingEnabled
Definition: ADCCC26XX.h:146
ADCCC26XX_Sampling_Duration samplingDuration
Definition: ADCCC26XX.h:148
Definition: ADCCC26XX.h:131
Definition: ADCCC26XX.h:87
Generic PIN & GPIO driver.
Definition: ADCCC26XX.h:92
ADCCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCCC26XX.h:119
Definition: ADCCC26XX.h:121