![]() |
![]() |
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
Driver for the Bosch BMP280 Pressure Sensor.
============================================================================
#include "stdint.h"
#include "stdbool.h"
Go to the source code of this file.
Macros | |
#define | SENSOR_BMP280_DATASIZE 6 |
Functions | |
bool | SensorBmp280_init (void) |
void | SensorBmp280_enable (bool enable) |
bool | SensorBmp280_test (void) |
bool | SensorBmp280_read (uint8_t *pBuf) |
void | SensorBmp280_convert (uint8_t *raw, int32_t *temp, uint32_t *press) |
#define SENSOR_BMP280_DATASIZE 6 |
bool SensorBmp280_init | ( | void | ) |
void SensorBmp280_enable | ( | bool | enable | ) |
bool SensorBmp280_test | ( | void | ) |
bool SensorBmp280_read | ( | uint8_t * | pBuf | ) |
void SensorBmp280_convert | ( | uint8_t * | raw, |
int32_t * | temp, | ||
uint32_t * | press | ||
) |