111 #ifndef ti_drivers_UDMACC26XX__include
112 #define ti_drivers_UDMACC26XX__include
125 #undef DEVICE_FAMILY_PATH
126 #define DEVICE_FAMILY_PATH(x) <ti/devices/DEVICE_FAMILY/x>
127 #include DEVICE_FAMILY_PATH(inc/hw_types.h)
128 #include DEVICE_FAMILY_PATH(driverlib/udma.h)
130 #error "You must define DEVICE_FAMILY at the project level as one of cc26x0, cc26x0r2, cc13x0, etc."
161 #ifndef UDMACC26XX_CONFIG_BASE
162 #define UDMACC26XX_CONFIG_BASE 0x20000400
166 #if(UDMACC26XX_CONFIG_BASE & 0x3FF)
167 #error "Base address for DMA control table 'UDMACC26XX_CONFIG_BASE' must be 1024 bytes aligned."
171 #if defined(__IAR_SYSTEMS_ICC__)
172 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
173 __no_init static volatile tDMAControlTable ENTRY_NAME @ UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable)
174 #elif defined(__TI_COMPILER_VERSION__)
175 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
176 PRAGMA(LOCATION( ENTRY_NAME , UDMACC26XX_CONFIG_BASE + CHANNEL_INDEX * sizeof(tDMAControlTable) );)\
177 static volatile tDMAControlTable ENTRY_NAME
178 #define PRAGMA(x) _Pragma(#x)
179 #elif defined(__GNUC__)
180 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \
181 extern int UDMACC26XX_ ## ENTRY_NAME ## _is_placed; __attribute__ ((section("."#ENTRY_NAME))) static volatile tDMAControlTable ENTRY_NAME = {&UDMACC26XX_ ## ENTRY_NAME ## _is_placed}
183 #error "don't know how to define ALLOCATE_CONTROL_TABLE_ENTRY for this toolchain"
187 #define UDMACC26XX_SET_TRANSFER_SIZE(SIZE) (((SIZE - 1) << UDMA_XFER_SIZE_S) & UDMA_XFER_SIZE_M)
189 #define UDMACC26XX_GET_TRANSFER_SIZE(CONTROL) (((CONTROL & UDMA_XFER_SIZE_M) >> UDMA_XFER_SIZE_S) + 1)
196 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
268 object->isOpen = FALSE;
309 HWREG(hwAttrs->
baseAddr + UDMA_O_SETCHANNELEN) = channelBitMask;
338 return (uDMAIntStatus(hwAttrs->
baseAddr) & channelBitMask) ?
true :
false;
366 uDMAIntClear(hwAttrs->
baseAddr, channelBitMask);
394 uDMAChannelDisable(hwAttrs->
baseAddr, channelBitMask);
bool isOpen
Definition: UDMACC26XX.h:195
PowerCC26XX_Resource powerMngrId
Definition: UDMACC26XX.h:204
void UDMACC26XX_close(UDMACC26XX_Handle handle)
Function to close the DMA driver.
__STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:358
__STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:301
uint8_t intNum
Definition: UDMACC26XX.h:205
__STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
Function to initialize the CC26XX DMA driver.
Definition: UDMACC26XX.h:260
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:235
Power manager interface for CC26XX/CC13XX.
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: UDMACC26XX.h:196
struct UDMACC26XX_Object UDMACC26XX_Object
UDMACC26XX object.
UDMACC26XX_Handle UDMACC26XX_open()
Function to initialize the CC26XX DMA peripheral.
struct UDMACC26XX_Config UDMACC26XX_Config
UDMACC26XX Global configuration.
UDMACC26XX hardware attributes.
Definition: UDMACC26XX.h:202
void * object
Definition: UDMACC26XX.h:236
uint8_t intPriority
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority...
Definition: UDMACC26XX.h:229
__STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:386
__STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:330
uint32_t baseAddr
Definition: UDMACC26XX.h:203
void UDMACC26XX_hwiIntFxn(UArg callbacks)
UDMACC26XX object.
Definition: UDMACC26XX.h:194
struct UDMACC26XX_Config * UDMACC26XX_Handle
A handle that is returned from a UDMACC26XX_open() call.
Definition: UDMACC26XX.h:243
void const * hwAttrs
Definition: UDMACC26XX.h:237
struct UDMACC26XX_HWAttrs UDMACC26XX_HWAttrs
UDMACC26XX hardware attributes.