![]() |
![]() |
|
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
Timer driver interface.
============================================================================
The Timer header file should be included in an application as follows:
The Timer driver operates as a generic timer interface for timing interval handling. It can be configured to run in one-shot blocking mode, one-shot callback mode, continuous callback mode, or free-run mode. This driver does not have PWM or capture functionalities. These functionalities are addressed in both the Capture and PWM driver modules.
The Timer driver also handles the general purpose timer resource allocation. For the driver that requires to use the general purpose timer, it calls Timer_open() to occupy the specified timer, and calls Timer_close() to release the occupied timer resource.
This module serves as the main interface for TI Drivers applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to a Timer_FxnTable.
The Timer driver interface module is joined (at link time) to a NULL-terminated array of Timer_Config data structures named Timer_config. Timer_config is implemented in the application with each entry being an instance of a Timer peripheral. Each entry in Timer_config contains a:
The Timer driver interface produces log statements if instrumentation is enabled.
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
| struct | Timer_Params_ |
| Timer Parameters. More... | |
| struct | Timer_FxnTable_ |
| The definition of a Timer function table that contains the required set of functions to control a specific Timer driver implementation. More... | |
| struct | Timer_Config_ |
Macros | |
| #define | TIMER_CMD_RESERVED (32) |
| #define | TIMER_STATUS_RESERVED (-32) |
| #define | TIMER_STATUS_SUCCESS (0) |
| Successful status code returned by Timer_control(). More... | |
| #define | TIMER_STATUS_ERROR (-1) |
| Generic error status code returned by Timer_control(). More... | |
| #define | TIMER_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by Timer_control() for undefined command codes. More... | |
Typedefs | |
| typedef struct Timer_Config_ * | Timer_Handle |
| A handle that is returned from a Timer_open() call. More... | |
| typedef enum Timer_Mode_ | Timer_Mode |
| Timer mode enum. More... | |
| typedef enum Timer_Period_Units_ | Timer_Period_Units |
| Timer period unit enum. More... | |
| typedef void(* | Timer_CallBackFxn) (Timer_Handle handle) |
| Timer callback function. More... | |
| typedef struct Timer_Params_ | Timer_Params |
| Timer Parameters. More... | |
| typedef int_fast16_t(* | Timer_ControlFxn) (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of Timer_control(). More... | |
| typedef void(* | Timer_CloseFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_close(). More... | |
| typedef uint32_t(* | Timer_GetCountFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_getCount(). More... | |
| typedef void(* | Timer_InitFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_init(). More... | |
| typedef Timer_Handle(* | Timer_OpenFxn) (Timer_Handle handle, Timer_Params *params) |
| A function pointer to a driver specific implementation of Timer_open(). More... | |
| typedef void(* | Timer_StartFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_start(). More... | |
| typedef void(* | Timer_StopFxn) (Timer_Handle handle) |
| A function pointer to a driver specific implementation of Timer_stop(). More... | |
| typedef struct Timer_FxnTable_ | Timer_FxnTable |
| The definition of a Timer function table that contains the required set of functions to control a specific Timer driver implementation. More... | |
| typedef struct Timer_Config_ | Timer_Config |
Enumerations | |
| enum | Timer_Mode_ { TIMER_ONESHOT_CB, TIMER_ONESHOT_BLOCK, TIMER_CONTINUOUS_CB, TIMER_MODE_FREE_RUNNING } |
| Timer mode enum. More... | |
| enum | Timer_Period_Units_ { TIMER_PERIOD_US, TIMER_PERIOD_HZ, TIMER_PERIOD_COUNTS } |
| Timer period unit enum. More... | |
Functions | |
| int_fast16_t | Timer_control (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given Timer_Handle. More... | |
| void | Timer_close (Timer_Handle handle) |
| Function to close a Timer peripheral specified by the Timer handle. More... | |
| uint32_t | Timer_getCount (Timer_Handle handle) |
| Function to get the current count of a started timer. More... | |
| void | Timer_init (void) |
| Function to initialize a timer module. This function will go through all available hardware resources and mark them as "available". More... | |
| Timer_Handle | Timer_open (uint_least8_t index, Timer_Params *params) |
| Function to initialize a given Timer peripheral specified by the particular index value. The parameter specifies which mode the Timer will operate. More... | |
| void | Timer_Params_init (Timer_Params *params) |
| Function to initialize the Timer_Params struct to its defaults. More... | |
| void | Timer_start (Timer_Handle handle) |
| Function to start Timer with the given period. The timer running mode and interval period unit are specified in the Timer_Params when calling Timer_open(). More... | |
| void | Timer_stop (Timer_Handle handle) |
| Function to stop timer after Timer_start() is called with success. More... | |
| #define TIMER_CMD_RESERVED (32) |
Common Timer_control command code reservation offset. Timer driver implementations should offset command codes with TIMER_CMD_RESERVED growing positively
Example implementation specific command codes:
| #define TIMER_STATUS_RESERVED (-32) |
Common Timer_control status code reservation offset. Timer driver implementations should offset status codes with TIMER_STATUS_RESERVED growing negatively.
Example implementation specific status codes:
| #define TIMER_STATUS_SUCCESS (0) |
Successful status code returned by Timer_control().
Timer_control() returns TIMER_STATUS_SUCCESS if the control code was executed successfully.
| #define TIMER_STATUS_ERROR (-1) |
Generic error status code returned by Timer_control().
Timer_control() returns TIMER_STATUS_ERROR if the control code was not executed successfully.
| #define TIMER_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by Timer_control() for undefined command codes.
Timer_control() returns TIMER_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
| typedef struct Timer_Config_* Timer_Handle |
A handle that is returned from a Timer_open() call.
| typedef enum Timer_Mode_ Timer_Mode |
Timer mode enum.
The Timer mode needs to be passed in Timer_open() to specify the timer running mode which handles the interrupt differently.
| typedef enum Timer_Period_Units_ Timer_Period_Units |
Timer period unit enum.
The Timer period unit needs to be passed in Timer_open() to specify the unit of timing interval.
| typedef void(* Timer_CallBackFxn) (Timer_Handle handle) |
Timer callback function.
User definable callback function prototype. The Timer driver will call the defined function and pass in the Timer driver's handle and the pointer to the user-specified the argument.
| handle | Timer_Handle |
| typedef struct Timer_Params_ Timer_Params |
Timer Parameters.
Timer parameters are used to with the Timer_open() call. Default values for these parameters are set using Timer_Params_init().
| typedef int_fast16_t(* Timer_ControlFxn) (Timer_Handle handle, uint_fast16_t cmd, void *arg) |
A function pointer to a driver specific implementation of Timer_control().
| typedef void(* Timer_CloseFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_close().
| typedef uint32_t(* Timer_GetCountFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_getCount().
| typedef void(* Timer_InitFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_init().
| typedef Timer_Handle(* Timer_OpenFxn) (Timer_Handle handle, Timer_Params *params) |
A function pointer to a driver specific implementation of Timer_open().
| typedef void(* Timer_StartFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_start().
| typedef void(* Timer_StopFxn) (Timer_Handle handle) |
A function pointer to a driver specific implementation of Timer_stop().
| typedef struct Timer_FxnTable_ Timer_FxnTable |
The definition of a Timer function table that contains the required set of functions to control a specific Timer driver implementation.
| typedef struct Timer_Config_ Timer_Config |
| enum Timer_Mode_ |
Timer mode enum.
The Timer mode needs to be passed in Timer_open() to specify the timer running mode which handles the interrupt differently.
| enum Timer_Period_Units_ |
Timer period unit enum.
The Timer period unit needs to be passed in Timer_open() to specify the unit of timing interval.
| Enumerator | |
|---|---|
| TIMER_PERIOD_US | |
| TIMER_PERIOD_HZ | |
| TIMER_PERIOD_COUNTS | |
| int_fast16_t Timer_control | ( | Timer_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given Timer_Handle.
| handle | A Timer_Handle returned from Timer_open(). |
| cmd | A command value defined by the driver specific implementation. |
| arg | A pointer to an optional R/W (read/write) argument that is accompanied with cmd. |
| void Timer_close | ( | Timer_Handle | handle | ) |
Function to close a Timer peripheral specified by the Timer handle.
The function takes care of timer resource allocation. The corresponding timer resource to the Timer_Handle is released to be an available timer resource.
| handle | A Timer_Handle returned from Timer_open |
| uint32_t Timer_getCount | ( | Timer_Handle | handle | ) |
Function to get the current count of a started timer.
| handle | A Timer_Handle returned from Timer_open |
| void Timer_init | ( | void | ) |
Function to initialize a timer module. This function will go through all available hardware resources and mark them as "available".
| Timer_Handle Timer_open | ( | uint_least8_t | index, |
| Timer_Params * | params | ||
| ) |
Function to initialize a given Timer peripheral specified by the particular index value. The parameter specifies which mode the Timer will operate.
The function takes care of timer resource allocation. If the particular timer passed by user has already been used by other modules, the return value is NULL. If the particular timer is available to use, Timer module owns it and returns a Timer_Handle.
| index | Logical peripheral number for the Timer indexed into the Timer_config table |
| params | Pointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only). |
| void Timer_Params_init | ( | Timer_Params * | params | ) |
Function to initialize the Timer_Params struct to its defaults.
| params | An pointer to Timer_Params structure for initialization |
Defaults values are: mode = TIMER_MODE_ONESHOT_BLOCKING callbackFxn = NULL periodUnit = TIMER_PERIOD_US period = 0xFFFF
| void Timer_start | ( | Timer_Handle | handle | ) |
Function to start Timer with the given period. The timer running mode and interval period unit are specified in the Timer_Params when calling Timer_open().
| handle | Timer_Handle |
| void Timer_stop | ( | Timer_Handle | handle | ) |
Function to stop timer after Timer_start() is called with success.
| handle | Timer_Handle |