SimpleLink MCU SDK Driver APIs  tidrivers_cc13xx_cc26xx_3_01_01_03
DisplayHost.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_display_DisplayHost__include
34 #define ti_display_DisplayHost__include
35 
36 #ifdef __cplusplus
37 extern "C"
38 {
39 #endif
40 
41 #include <ti/display/Display.h>
42 
43 typedef struct DisplayHost_HWAttrs
44 {
45  char *strBuf;
46  uint16_t strBufLen;
48 
49 typedef struct DisplayHost_Object
50 {
51  int dummy;
53 
54 
56 
57 
58 /* functions functions */
59 void DisplayHost_init(Display_Handle handle);
61  Display_Params * params);
63 void DisplayHost_clearLines(Display_Handle handle, uint8_t fromLine,
64  uint8_t toLine);
65 void DisplayHost_vprintf(Display_Handle handle, uint8_t line,
66  uint8_t column, char *fmt, va_list va);
68 int DisplayHost_control(Display_Handle handle, unsigned int cmd, void *arg);
69 unsigned int DisplayHost_getType(void);
70 #ifdef __cplusplus
71 }
72 #endif
73 
74 #endif /* ti_display_DisplayHost__include */
void DisplayHost_clear(Display_Handle handle)
unsigned int DisplayHost_getType(void)
int dummy
Definition: DisplayHost.h:51
uint16_t strBufLen
Definition: DisplayHost.h:46
Definition: DisplayHost.h:49
Display Parameters.
Definition: Display.h:442
void DisplayHost_vprintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
struct DisplayHost_HWAttrs DisplayHost_HWAttrs
Display_Handle DisplayHost_open(Display_Handle, Display_Params *params)
Generic interface for text output.
Definition: DisplayHost.h:43
struct DisplayHost_Object DisplayHost_Object
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:501
struct DisplayHost_Object * DisplayHost_Handle
void DisplayHost_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
char * strBuf
Definition: DisplayHost.h:45
Display Global configuration.
Definition: Display.h:524
void DisplayHost_close(Display_Handle)
const Display_FxnTable DisplayHost_fxnTable
int DisplayHost_control(Display_Handle handle, unsigned int cmd, void *arg)
void DisplayHost_init(Display_Handle handle)
Copyright 2016, Texas Instruments Incorporated