115 #ifndef ti_display_DisplayExt__include
116 #define ti_display_DisplayExt__include
123 #include <ti/grlib/grlib.h>
134 #if !defined(Display_DISABLE_ALL) || (!Display_DISABLE_ALL)
136 # define DisplayExt_getGraphicsContext(handle) \
137 DisplayExt_doGetGraphicsContext(handle)
139 # define DisplayExt_getGraphicsContext(handle) NULL
173 #endif //ti_display_DisplayExt__include
struct DisplayGrLib_Object * DisplayGrLib_Handle
Generic interface for text output.
Graphics_Context * DisplayExt_doGetGraphicsContext(Display_Handle handle)
Get the Graphics_Context object of the first available and open Display that uses GrLib for output...
struct DisplayGrLib_Object DisplayGrLib_Object
Graphics_Context g_sContext
Definition: DisplayExt.h:148
Display Global configuration.
Definition: Display.h:524
Definition: DisplayExt.h:146