344 #ifndef ti_drivers_uart_UARTCC26XX__include
345 #define ti_drivers_uart_UARTCC26XX__include
359 #undef DEVICE_FAMILY_PATH
360 #define DEVICE_FAMILY_PATH(x) <ti/devices/DEVICE_FAMILY/x>
362 #error "You must define DEVICE_FAMILY at the project level as one of cc26x0, cc26x0r2, cc13x0, etc."
365 #include DEVICE_FAMILY_PATH(driverlib/uart.h)
371 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
372 #include <ti/sysbios/family/arm/m3/Hwi.h>
373 #include <ti/sysbios/knl/Swi.h>
374 #include <ti/sysbios/knl/Clock.h>
375 #include <ti/sysbios/knl/Semaphore.h>
408 #define UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE UART_CMD_RESERVED + 0
417 #define UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE UART_CMD_RESERVED + 1
425 #define UARTCC26XX_CMD_RX_FIFO_FLUSH UART_CMD_RESERVED + 2
429 #define UARTCC26XX_FIFO_SIZE 32
432 #define UARTCC26XX_RETURN_PARTIAL_ENABLE UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE
433 #define UARTCC26XX_RETURN_PARTIAL_DISABLE UARTCC26XX_CMD_RETURN_PARTIAL_DISABLE
592 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
602 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
uint8_t rtsPin
Definition: UARTCC26XX.h:505
UARTCC26XX Hardware attributes.
Definition: UARTCC26XX.h:479
UART_Mode readMode
Definition: UARTCC26XX.h:545
Definition: UARTCC26XX.h:516
Power_NotifyObj uartPostObj
Definition: UARTCC26XX.h:589
uint32_t baudRate
Baud rate for CC26xx UART.
Definition: UARTCC26XX.h:561
const void * writeBuf
Definition: UARTCC26XX.h:568
size_t writeSize
Definition: UARTCC26XX.h:570
Definition: UARTCC26XX.h:534
enum UART_PAR_ UART_PAR
UART parity type settings.
enum UART_LEN_ UART_LEN
UART data length settings.
const UART_FxnTable UARTCC26XX_fxnTable
RingBuf_Object ringBuffer
Definition: UARTCC26XX.h:580
enum UART_Mode_ UART_Mode
UART mode settings.
Definition: UARTCC26XX.h:530
Power notify object structure.
Definition: Power.h:113
uint8_t writeFifoThreshold
Definition: UARTCC26XX.h:579
size_t readSize
Definition: UARTCC26XX.h:577
Definition: UARTCC26XX.h:518
unsigned int readTimeout
Definition: UARTCC26XX.h:547
bool readRetPartial
Definition: UARTCC26XX.h:574
void * uartPostFxn
Definition: UARTCC26XX.h:587
UART_ReturnMode readReturnMode
Definition: UARTCC26XX.h:551
UART_Status
UART status.
Definition: UARTCC26XX.h:515
Semaphore_Struct writeSem
Definition: UARTCC26XX.h:594
Definition: UARTCC26XX.h:520
UARTCC26XX Object.
Definition: UARTCC26XX.h:542
UART_Callback readCallback
Definition: UARTCC26XX.h:549
Swi_Struct swi
Definition: UARTCC26XX.h:593
UART_PAR parityType
Definition: UARTCC26XX.h:564
Definition: UARTCC26XX.h:519
size_t readCount
Definition: UARTCC26XX.h:576
UART_LEN dataLength
Definition: UARTCC26XX.h:562
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: UARTCC26XX.h:592
Definition: UARTCC26XX.h:532
UART_FifoThreshold readFifoThreshold
Definition: UARTCC26XX.h:578
Device-specific pin & GPIO driver for CC26xx family [def].
struct UARTCC26XX_HWAttrsV2 UARTCC26XX_HWAttrsV2
UARTCC26XX Hardware attributes.
Semaphore_Struct readSem
Definition: UARTCC26XX.h:595
uint32_t baseAddr
Definition: UARTCC26XX.h:480
int intNum
Definition: UARTCC26XX.h:482
UART_Status status
Definition: UARTCC26XX.h:565
Definition: UARTCC26XX.h:521
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:648
size_t writeCount
Definition: UARTCC26XX.h:569
unsigned int writeTimeout
Definition: UARTCC26XX.h:548
bool opened
Definition: UARTCC26XX.h:544
uint8_t intPriority
UART Peripheral's interrupt priority.
Definition: UARTCC26XX.h:495
size_t ringBufSize
Definition: UARTCC26XX.h:507
uint8_t rxPin
Definition: UARTCC26XX.h:503
unsigned char * ringBufPtr
Definition: UARTCC26XX.h:506
UART_STOP stopBits
Definition: UARTCC26XX.h:563
bool writeCR
Definition: UARTCC26XX.h:571
Definition: UARTCC26XX.h:517
Definition: UARTCC26XX.h:533
underlying data structure for type PIN_State
Definition: PIN.h:687
UART_Mode writeMode
Definition: UARTCC26XX.h:546
enum UART_STOP_ UART_STOP
UART stop bit settings.
enum UART_ReturnMode_ UART_ReturnMode
UART return mode settings.
void * readBuf
Definition: UARTCC26XX.h:575
UART_DataMode readDataMode
Definition: UARTCC26XX.h:552
struct UARTCC26XX_Object * UARTCC26XX_Handle
UART_DataMode writeDataMode
Definition: UARTCC26XX.h:553
PIN_State pinState
Definition: UARTCC26XX.h:583
uint8_t ctsPin
Definition: UARTCC26XX.h:504
struct UARTCC26XX_Object UARTCC26XX_Object
UARTCC26XX Object.
Definition: UARTCC26XX.h:531
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: UARTCC26XX.h:501
UART_Callback writeCallback
Definition: UARTCC26XX.h:550
Clock_Struct txFifoEmptyClk
Definition: UARTCC26XX.h:596
uint32_t powerMngrId
Definition: UARTCC26XX.h:481
PIN_Handle hPin
Definition: UARTCC26XX.h:584
UART_FifoThreshold
UART FIFO threshold.
Definition: UARTCC26XX.h:529
void(* UART_Callback)(UART_Handle handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:434
uint8_t txPin
Definition: UARTCC26XX.h:502
enum UART_DataMode_ UART_DataMode
UART data mode settings.