490 #ifndef ti_drivers_spi_SPICC26XXDMA__include
491 #define ti_drivers_spi_SPICC26XXDMA__include
504 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
505 #include <ti/sysbios/knl/Semaphore.h>
506 #include <ti/sysbios/knl/Swi.h>
507 #include <ti/sysbios/family/arm/m3/Hwi.h>
540 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0)
549 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1)
557 #define SPICC26XXDMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2)
568 #define SPICC26XXDMA_CMD_SET_CSN_WAKEUP (SPI_CMD_RESERVED + 3)
572 #define SPICC26XXDMA_RETURN_PARTIAL_ENABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE
573 #define SPICC26XXDMA_RETURN_PARTIAL_DISABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE
574 #define SPICC26XXDMA_SET_CSN_PIN SPICC26XXDMA_CMD_SET_CSN_PIN
575 #define SPICC26XXDMA_SET_CSN_WAKEUP SPICC26XXDMA_CMD_SET_CSN_WAKEUP
727 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
747 #ifdef SPICC26XXDMA_WAKEUP_ENABLED
766 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
Definition: SPICC26XXDMA.h:595
uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:557
PIN_Id csnPin
Definition: SPICC26XXDMA.h:736
const SPI_FxnTable SPICC26XXDMA_fxnTable
uint16_t defaultTxBufValue
Definition: SPICC26XXDMA.h:690
uint32_t baseAddr
Definition: SPICC26XXDMA.h:664
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:540
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation.
Power_NotifyObj spiPostObj
Definition: SPICC26XXDMA.h:757
unsigned int bitRate
SPI bit rate in Hz.
Definition: SPICC26XXDMA.h:722
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:522
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26XXDMA.h:714
struct SPICC26XXDMA_Object * SPICC26XXDMA_Handle
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26XXDMA.h:680
Semaphore_Struct transferComplete
Definition: SPICC26XXDMA.h:729
uint32_t rxChannelBitMask
Definition: SPICC26XXDMA.h:692
void * spiPreFxn
Definition: SPICC26XXDMA.h:754
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:235
uint32_t txChannelBitMask
Definition: SPICC26XXDMA.h:694
uint16_t scratchBuf
Definition: SPICC26XXDMA.h:751
Power manager interface for CC26XX/CC13XX.
Power notify object structure.
Definition: Power.h:113
PIN_Id clkPin
Definition: SPICC26XXDMA.h:700
SPICC26XXDMA Hardware attributes.
Definition: SPICC26XXDMA.h:662
volatile bool spiPowerConstraint
Definition: SPICC26XXDMA.h:759
PIN_Id misoPin
Definition: SPICC26XXDMA.h:698
SPI_TransferMode transferMode
Definition: SPICC26XXDMA.h:712
SPICC26XXDMA Object.
Definition: SPICC26XXDMA.h:710
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Device-specific pin & GPIO driver for CC26xx family [def].
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:652
void * spiPostFxn
Definition: SPICC26XXDMA.h:755
PIN_State pinState
Definition: SPICC26XXDMA.h:739
SPI_Mode mode
Definition: SPICC26XXDMA.h:715
SPICC26XXDMA_FrameSize
Definition: SPICC26XXDMA.h:594
SPICC26XXDMA_FrameSize frameSize
Definition: SPICC26XXDMA.h:733
UDMACC26XX driver implementation.
bool returnPartial
Definition: SPICC26XXDMA.h:746
struct SPICC26XXDMA_Object SPICC26XXDMA_Object
SPICC26XXDMA Object.
struct SPICC26XXDMA_HWAttrsV1 SPICC26XXDMA_HWAttrsV1
SPICC26XXDMA Hardware attributes.
SPI Global configuration.
Definition: SPI.h:683
PIN_Id csnPin
Definition: SPICC26XXDMA.h:702
UDMACC26XX_Handle udmaHandle
Definition: SPICC26XXDMA.h:743
uint8_t intNum
Definition: SPICC26XXDMA.h:666
PIN_Id mosiPin
Definition: SPICC26XXDMA.h:696
unsigned int transferTimeout
Definition: SPICC26XXDMA.h:713
underlying data structure for type PIN_State
Definition: PIN.h:687
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
SPI_FrameFormat frameFormat
Definition: SPICC26XXDMA.h:724
Power_NotifyObj spiPreObj
Definition: SPICC26XXDMA.h:756
bool isOpen
Definition: SPICC26XXDMA.h:761
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: SPICC26XXDMA.h:727
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26XXDMA.h:686
void(* SPICC26XXDMA_CallbackFxn)(SPI_Handle handle)
Definition: SPICC26XXDMA.h:606
Definition: SPICC26XXDMA.h:596
PowerCC26XX_Resource powerMngrId
Definition: SPICC26XXDMA.h:688
PIN_Handle pinHandle
Definition: SPICC26XXDMA.h:740
unsigned int dataSize
Definition: SPICC26XXDMA.h:723
SPI_Transaction * currentTransaction
Definition: SPICC26XXDMA.h:732
Swi_Struct swi
Definition: SPICC26XXDMA.h:728