52 #ifndef ti_drivers_power_PowerCC26XX_
53 #define ti_drivers_power_PowerCC26XX_
59 #include <ti/sysbios/family/arm/m3/Hwi.h>
60 #include <ti/sysbios/knl/Clock.h>
64 typedef uint8_t PowerCC26XX_Resource;
68 #define PowerCC26XX_RESUMETIMESTANDBY 750
71 #define PowerCC26XX_TOTALTIMESTANDBY 1000
74 #define PowerCC26XX_WAKEDELAYSTANDBY 130
77 #define PowerCC26XX_INITIALWAITRCOSC_LF 1000
80 #define PowerCC26XX_RETRYWAITRCOSC_LF 1000
83 #define PowerCC26XX_INITIALWAITXOSC_HF 50
86 #define PowerCC26XX_RETRYWAITXOSC_HF 50
89 #define PowerCC26XX_INITIALWAITXOSC_LF 10000
92 #define PowerCC26XX_RETRYWAITXOSC_LF 5000
95 #define PowerCC26XX_PERIPH_GPT0 0
98 #define PowerCC26XX_PERIPH_GPT1 1
101 #define PowerCC26XX_PERIPH_GPT2 2
104 #define PowerCC26XX_PERIPH_GPT3 3
107 #define PowerCC26XX_PERIPH_SSI0 4
110 #define PowerCC26XX_PERIPH_SSI1 5
113 #define PowerCC26XX_PERIPH_UART0 6
115 #define PowerCC26XX_PERIPH_I2C0 7
117 #define PowerCC26XX_PERIPH_TRNG 8
120 #define PowerCC26XX_PERIPH_GPIO 9
122 #define PowerCC26XX_PERIPH_UDMA 10
124 #define PowerCC26XX_PERIPH_CRYPTO 11
126 #define PowerCC26XX_PERIPH_I2S 12
128 #define PowerCC26XX_PERIPH_RFCORE 13
130 #define PowerCC26XX_XOSC_HF 14
133 #define PowerCC26XX_DOMAIN_PERIPH 15
136 #define PowerCC26XX_DOMAIN_SERIAL 16
139 #define PowerCC26XX_DOMAIN_RFCORE 17
142 #define PowerCC26XX_DOMAIN_SYSBUS 18
146 #define PowerCC26XX_NUMRESOURCES 19
151 #define PowerCC26XX_PERIPH 0x80
152 #define PowerCC26XX_SPECIAL 0x40
153 #define PowerCC26XX_DOMAIN 0x00
154 #define PowerCC26XX_PARENTMASK 0x3F
155 #define PowerCC26XX_NOPARENT 0x3F
158 #define PowerCC26XX_STANDBY 0x1
161 #define PowerCC26XX_ENABLE 1
162 #define PowerCC26XX_DISABLE 0
166 #define PowerCC26XX_SB_VIMS_CACHE_RETAIN 0
169 #define PowerCC26XX_SD_DISALLOW 1
172 #define PowerCC26XX_SB_DISALLOW 2
175 #define PowerCC26XX_IDLE_PD_DISALLOW 3
178 #define PowerCC26XX_NEED_FLASH_IN_IDLE 4
182 #define PowerCC26XX_NUMCONSTRAINTS 5
191 #define PowerCC26XX_ENTERING_STANDBY 0x1
194 #define PowerCC26XX_ENTERING_SHUTDOWN 0x2
197 #define PowerCC26XX_AWAKE_STANDBY 0x4
200 #define PowerCC26XX_AWAKE_STANDBY_LATE 0x8
203 #define PowerCC26XX_XOSC_HF_SWITCHED 0x10
207 #define PowerCC26XX_NUMEVENTS 5
214 #define PowerCC26XX_SETUP_CALIBRATE 1
215 #define PowerCC26XX_INITIATE_CALIBRATE 2
216 #define PowerCC26XX_DO_CALIBRATE 3
221 typedef struct PowerCC26XX_ResourceRecord {
224 uint16_t driverlibID;
225 } PowerCC26XX_ResourceRecord;
459 #define Power_getPerformanceLevel(void) 0
460 #define Power_setPerformanceLevel(level) Power_EFAIL
Hwi_Struct hwiStruct
Definition: PowerCC26XX.h:317
bool calLF
Definition: PowerCC26XX.h:329
void PowerCC26XX_doWFI(void)
The Wait for interrupt (WFI) policy.
int32_t nDeltaFreqNew
Definition: PowerCC26XX.h:325
bool xoscPending
Definition: PowerCC26XX.h:328
struct PowerCC26XX_Config PowerCC26XX_Config
Global configuration structure.
bool bRefine
Definition: PowerCC26XX.h:326
bool PowerCC26XX_calibrate(unsigned int arg)
The RC Oscillator (RCOSC) calibration function.
uint32_t constraintMask
Definition: PowerCC26XX.h:312
bool calibrateRCOSC_LF
Boolean specifying whether the low frequency RC oscillator (RCOSC_LF) should be calibrated.
Definition: PowerCC26XX.h:292
Clock_Handle PowerCC26XX_getClockHandle(void)
Get the handle of the Clock object used for scheduling device wakeups.
struct PowerCC26XX_ModuleState PowerCC26XX_ModuleState
PowerCC26XX_ModuleState.
Power_PolicyInitFxn policyInitFxn
The Power Policy's initialization function.
Definition: PowerCC26XX.h:236
void(* Power_PolicyInitFxn)(void)
Power policy initialization function pointer.
Definition: Power.h:92
uint8_t resourceCounts[PowerCC26XX_NUMRESOURCES]
Definition: PowerCC26XX.h:338
bool enablePolicy
Boolean specifying if the Power Policy function is enabled.
Definition: PowerCC26XX.h:283
int32_t nCtrimFractNew
Definition: PowerCC26XX.h:322
Power_PolicyFxn policyFxn
The Power Policy function.
Definition: PowerCC26XX.h:258
bool initialized
Definition: PowerCC26XX.h:335
int32_t nRtrimNew
Definition: PowerCC26XX.h:323
int32_t nCtrimNew
Definition: PowerCC26XX.h:321
unsigned int(* resourceHandlers[3])(unsigned int)
Definition: PowerCC26XX.h:340
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:97
uint32_t state
Definition: PowerCC26XX.h:327
bool busyCal
Definition: PowerCC26XX.h:331
void PowerCC26XX_standbyPolicy(void)
The STANDBY Power Policy.
void PowerCC26XX_switchXOSC_HF(void)
Switch the HF clock source to XOSC_HF.
bool(* calibrateFxn)(unsigned int)
The function to be used for activating RC Oscillator (RCOSC) calibration.
Definition: PowerCC26XX.h:270
bool calibrateRCOSC_HF
Boolean specifying whether the high frequency RC oscillator (RCOSC_HF) should be calibrated.
Definition: PowerCC26XX.h:301
Power_PolicyFxn policyFxn
Definition: PowerCC26XX.h:342
uint32_t PowerCC26XX_getXoscStartupTime(uint32_t timeUntilWakeupInMs)
Get the estimated HF crystal oscillator (XOSC_HF) startup delay, for a given delay from now...
Clock_Struct calClockStruct
Definition: PowerCC26XX.h:316
int32_t nCtrimCurr
Definition: PowerCC26XX.h:319
PowerCC26XX_ModuleState.
Definition: PowerCC26XX.h:310
uint8_t calStep
Definition: PowerCC26XX.h:332
Global configuration structure.
Definition: PowerCC26XX.h:229
bool PowerCC26XX_injectCalibration(void)
Explicitly trigger RC oscillator calibration.
int32_t nCtrimFractCurr
Definition: PowerCC26XX.h:320
Clock_Struct lfClockObj
Definition: PowerCC26XX.h:315
int32_t nDeltaFreqCurr
Definition: PowerCC26XX.h:318
bool PowerCC26XX_noCalibrate(unsigned int arg)
Function to specify when RCOSC calibration is to be disabled.
bool firstLF
Definition: PowerCC26XX.h:333
int32_t nRtrimCurr
Definition: PowerCC26XX.h:324
Clock_Struct xoscClockObj
Definition: PowerCC26XX.h:314
bool enablePolicy
Definition: PowerCC26XX.h:334
uint8_t hwiState
Definition: PowerCC26XX.h:330
List_List notifyList
Definition: PowerCC26XX.h:311
uint8_t constraintCounts[PowerCC26XX_NUMCONSTRAINTS]
Definition: PowerCC26XX.h:336
Clock_Struct clockObj
Definition: PowerCC26XX.h:313