SimpleLink MCU SDK Driver APIs  tidrivers_cc13xx_cc26xx_3_01_01_03
Power.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2016, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
55 #ifndef ti_drivers_Power__include
56 #define ti_drivers_Power__include
57 
58 #include <stdint.h>
59 #include <ti/drivers/utils/List.h>
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 /* Power latency types */
66 #define Power_TOTAL (1U)
67 #define Power_RESUME (2U)
69 /* Power notify responses */
70 #define Power_NOTIFYDONE (0)
71 #define Power_NOTIFYERROR (-1)
73 /* Power status */
74 #define Power_SOK (0)
75 #define Power_EFAIL (-1)
76 #define Power_EINVALIDINPUT (-2)
77 #define Power_EINVALIDPOINTER (-3)
78 #define Power_ECHANGE_NOT_ALLOWED (-4)
79 #define Power_EBUSY (-5)
81 /* Power transition states */
82 #define Power_ACTIVE (1U)
83 #define Power_ENTERING_SLEEP (2U)
84 #define Power_EXITING_SLEEP (3U)
85 #define Power_ENTERING_SHUTDOWN (4U)
86 #define Power_CHANGING_PERF_LEVEL (5U)
92 typedef void (*Power_PolicyInitFxn)(void);
93 
97 typedef void (*Power_PolicyFxn)(void);
98 
102 typedef int_fast16_t (*Power_NotifyFxn)(uint_fast16_t eventType,
103  uintptr_t eventArg, uintptr_t clientArg);
104 
113 typedef struct Power_NotifyObj_ {
115  uint_fast16_t eventTypes;
117  uintptr_t clientArg;
119 
132 void Power_disablePolicy(void);
133 
153 void Power_enablePolicy(void);
154 
177 uint_fast32_t Power_getConstraintMask(void);
178 
196 int_fast16_t Power_getDependencyCount(uint_fast16_t resourceId);
197 
210 uint_fast16_t Power_getPerformanceLevel(void);
211 
233 uint_fast32_t Power_getTransitionLatency(uint_fast16_t sleepState,
234  uint_fast16_t type);
235 
249 uint_fast16_t Power_getTransitionState(void);
250 
261 void Power_idleFunc(void);
262 
273 int_fast16_t Power_init(void);
274 
335 int_fast16_t Power_registerNotify(Power_NotifyObj *pNotifyObj,
336  uint_fast16_t eventTypes,
337  Power_NotifyFxn notifyFxn,
338  uintptr_t clientArg);
339 
370 int_fast16_t Power_releaseConstraint(uint_fast16_t constraintId);
371 
390 int_fast16_t Power_releaseDependency(uint_fast16_t resourceId);
391 
414 int_fast16_t Power_setConstraint(uint_fast16_t constraintId);
415 
446 int_fast16_t Power_setDependency(uint_fast16_t resourceId);
447 
485 int_fast16_t Power_setPerformanceLevel(uint_fast16_t level);
486 
494 void Power_setPolicy(Power_PolicyFxn policy);
495 
537 int_fast16_t Power_shutdown(uint_fast16_t shutdownState,
538  uint_fast32_t shutdownTime);
539 
559 int_fast16_t Power_sleep(uint_fast16_t sleepState);
560 
572 void Power_unregisterNotify(Power_NotifyObj *pNotifyObj);
573 
574 #ifdef __cplusplus
575 }
576 #endif
577 
578 #endif /* ti_drivers_Power__include */
uint_fast32_t Power_getTransitionLatency(uint_fast16_t sleepState, uint_fast16_t type)
Get the hardware transition latency for a sleep state.
int_fast16_t Power_getDependencyCount(uint_fast16_t resourceId)
Get the current dependency count for a resource.
uintptr_t clientArg
Definition: Power.h:117
int_fast16_t Power_sleep(uint_fast16_t sleepState)
Transition the device into a sleep state.
int_fast16_t Power_init(void)
Power initialization function.
Power notify object structure.
Definition: Power.h:113
int_fast16_t(* Power_NotifyFxn)(uint_fast16_t eventType, uintptr_t eventArg, uintptr_t clientArg)
Power notify function pointer.
Definition: Power.h:102
int_fast16_t Power_setPerformanceLevel(uint_fast16_t level)
Set the MCU performance level.
int_fast16_t Power_setConstraint(uint_fast16_t constraintId)
Declare an operational constraint.
int_fast16_t Power_registerNotify(Power_NotifyObj *pNotifyObj, uint_fast16_t eventTypes, Power_NotifyFxn notifyFxn, uintptr_t clientArg)
Register a function to be called upon a specific power event.
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:97
int_fast16_t Power_shutdown(uint_fast16_t shutdownState, uint_fast32_t shutdownTime)
Put the device into a shutdown state.
Definition: List.h:126
uint_fast16_t Power_getPerformanceLevel(void)
Get the current performance level.
void Power_setPolicy(Power_PolicyFxn policy)
Set a new Power policy.
struct Power_NotifyObj_ Power_NotifyObj
Power notify object structure.
int_fast16_t Power_releaseDependency(uint_fast16_t resourceId)
Release a previously declared dependency.
void Power_unregisterNotify(Power_NotifyObj *pNotifyObj)
Unregister previously registered notifications.
uint_fast32_t Power_getConstraintMask(void)
Get the constraints that have been declared with Power.
void Power_disablePolicy(void)
Disable the configured power policy from running when the CPU is idle.
uint_fast16_t Power_getTransitionState(void)
Get the current transition state of the Power manager.
List_Elem link
Definition: Power.h:114
int_fast16_t Power_releaseConstraint(uint_fast16_t constraintId)
Release a previously declared constraint.
int_fast16_t Power_setDependency(uint_fast16_t resourceId)
Declare a dependency upon a resource.
void Power_enablePolicy(void)
Enable the configured power policy to run when the CPU is idle.
void Power_idleFunc(void)
Power function to be added to the application idle loop.
Power_NotifyFxn notifyFxn
Definition: Power.h:116
uint_fast16_t eventTypes
Definition: Power.h:115
Linked List interface for use in drivers.
Copyright 2016, Texas Instruments Incorporated