![]() |
![]() |
|
SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
I2S driver interface.
The I2S header file should be included in an application as follows:
The I2S driver facilitates the use of Inter-IC Sound (I2S), which is used to connect digital audio devices so that audio signals can be communicated between devices. The I2S driver simplifies reading and writing to any of the Multichannel Audio Serial Port (McASP) peripherals on the board with Receive and Transmit support. These include blocking, non-blocking, read and write characters on the McASP peripheral.
The APIs in this driver serve as an interface to a typical RTOS application. Its purpose is to redirect the I2S APIs to specific driver implementations which are specified using a pointer to an I2S_FxnTable. The specific peripheral implementations are responsible for creating all the RTOS specific primitives to allow for thread-safe operation.
To use the I2S driver for reaading and writing data to the I2S peripheral, the application calls the following APIs:
In order to use the I2S APIs, the application is required to provide device-specific I2S configuration in the Board.c file. The I2S driver interface defines a configuration data structure:
The application must declare an array of I2S_Config elements, named I2S_config[]. Each element of I2S_config[] must be populated with pointers to a device specific I2S driver implementation's function table, driver object, and hardware attributes. The hardware attributes define properties such as the I2S peripheral's base address and pins. Each element in I2S_config[] corresponds to an I2S instance, and and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as I2S0 or I2S1). For example, it is possible to use I2S_config[0] for I2S1.
Because I2S configuration is very device dependent, you will need to check the doxygen for the device specific I2S implementation. There you will find a description of the I2S hardware attributes. Please also refer to the board.c file of any of your examples to see the I2S configuration.
I2S_init() must be called before any other I2S APIs. This function iterates through the elements of the I2S_config[] array, calling the element's device implementation I2S initialization function.
The I2S_Params structure is passed to the I2S_open() call. If NULL is passed for the parameters, I2S_open() uses default parameters. An I2S_Params structure is initialized with default values by passing it to I2S_Params_init(). Some of the I2S parameters are described below. To see brief descriptions of all the parameters, see I2S_Params.
The I2S operation mode determines whether transmit and/or receive modes are enabled. The mode is specified with one of the following constants:
A separate data mode may be specified for read calls and write calls. The available modes are:
After initializing the I2S driver by calling I2S_init(), the application can open an I2S instance by calling I2S_open(). This function takes an index into the I2S_config[] array, and an I2S parameters data structure. The I2S instance is specified by the index of the I2S in I2S_config[]. Only one I2S index can be used at a time; calling I2S_open() a second time with the same index previosly passed to I2S_open() will result in an error. You can, though, re-use the index if the instance is closed via I2S_close().
If NULL is passed for the I2S_Params structure to I2S_open(), default values are used. If the open call is successful, it returns a non-NULL value.
Example opening an I2S driver instance:
The following example calls I2S_writeIssue() to write to an I2S driver instance that has been opened. It first queues up two buffers of text. Within an infinite loop, it calls I2S_writeReclaim() to retrieve a buffer and then re-queues the buffer.
The following example calls I2S_readIssue() to queue a buffer for reading from an I2S driver instance. It first queues up two buffers of text. Within an infinite loop, it then calls I2S_readReclaim() to retrieve a full buffer of data.
The I2S driver interface module is joined (at link time) to an array of I2S_Config data structures named I2S_config. I2S_config is implemented in the application with each entry being an instance of a I2S peripheral. Each entry in I2S_config contains a:

Go to the source code of this file.
Data Structures | |
| struct | I2S_BufDesc_ |
| I2S buffer descriptor for issue/reclaim mode. More... | |
| struct | I2S_Params_ |
| Basic I2S Parameters. More... | |
| struct | I2S_FxnTable_ |
| The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation. More... | |
| struct | I2S_Config_ |
| I2S Global configuration. More... | |
Macros | |
| #define | I2S_CMD_RESERVED (32) |
| #define | I2S_STATUS_RESERVED (-32) |
| #define | I2S_STATUS_SUCCESS (0) |
| Successful status code returned by I2S_control(). More... | |
| #define | I2S_STATUS_ERROR (-1) |
| Generic error status code returned by I2S_control(). More... | |
| #define | I2S_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by I2S_control() for undefined command codes. More... | |
| #define | I2S_ERROR (I2S_STATUS_ERROR) |
| #define | I2S_WAIT_FOREVER (~(0U)) |
| Wait forever define. More... | |
Typedefs | |
| typedef struct I2S_Config_ * | I2S_Handle |
| A handle that is returned from a I2S_open() call. More... | |
| typedef struct I2S_BufDesc_ | I2S_BufDesc |
| I2S buffer descriptor for issue/reclaim mode. More... | |
| typedef void(* | I2S_Callback) (I2S_Handle handle, I2S_BufDesc *desc) |
| The definition of a callback function used by the I2S driver when used in I2S_MODE_CALLBACK. More... | |
| typedef enum I2S_DataMode_ | I2S_DataMode |
| I2S mode settings. More... | |
| typedef enum I2S_OpMode_ | I2S_OpMode |
| I2S mode settings. More... | |
| typedef enum I2S_SerInActiveConfig_ | I2S_SerInActiveConfig |
| I2S Serializer InActive state settings. More... | |
| typedef enum I2S_PinMode_ | I2S_PinMode |
| I2S serial pin mode. More... | |
| typedef struct I2S_Params_ | I2S_Params |
| Basic I2S Parameters. More... | |
| typedef void(* | I2S_CloseFxn) (I2S_Handle handle) |
| A function pointer to a driver specific implementation of I2S_CloseFxn(). More... | |
| typedef int_fast16_t(* | I2S_ControlFxn) (I2S_Handle handle, uint_fast16_t cmd, void *arg) |
| A function pointer to a driver specific implementation of I2S_control(). More... | |
| typedef void(* | I2S_InitFxn) (I2S_Handle handle) |
| A function pointer to a driver specific implementation of I2S_init(). More... | |
| typedef I2S_Handle(* | I2S_OpenFxn) (I2S_Handle handle, I2S_Params *params) |
| A function pointer to a driver specific implementation of I2S_OpenFxn(). More... | |
| typedef int_fast16_t(* | I2S_IssueFxn) (I2S_Handle handle, I2S_BufDesc *desc) |
| A function pointer to a driver specific implementation of I2S_IssueFxn(). More... | |
| typedef size_t(* | I2S_ReclaimFxn) (I2S_Handle handle, I2S_BufDesc **desc) |
| A function pointer to a driver specific implementation of I2S_ReclaimFxn(). More... | |
| typedef struct I2S_FxnTable_ | I2S_FxnTable |
| The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation. More... | |
| typedef struct I2S_Config_ | I2S_Config |
| I2S Global configuration. More... | |
Enumerations | |
| enum | I2S_DataMode_ { I2S_MODE_CALLBACK, I2S_MODE_ISSUERECLAIM } |
| I2S mode settings. More... | |
| enum | I2S_OpMode_ { I2S_OPMODE_TX_ONLY, I2S_OPMODE_RX_ONLY, I2S_OPMODE_TX_RX_SYNC } |
| I2S mode settings. More... | |
| enum | I2S_SerInActiveConfig_ { I2S_SERCONFIG_INACT_TRI_STATE, I2S_SERCONFIG_INACT_LOW_LEVEL, I2S_SERCONFIG_INACT_HIGH_LEVEL } |
| I2S Serializer InActive state settings. More... | |
| enum | I2S_PinMode_ { I2S_PINMODE_RX, I2S_PINMODE_TX, I2S_PINMODE_INACTIVE } |
| I2S serial pin mode. More... | |
Functions | |
| void | I2S_close (I2S_Handle handle) |
| Function to close a given I2S peripheral specified by the I2S handle. More... | |
| int_fast16_t | I2S_control (I2S_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given I2S_Handle. More... | |
| void | I2S_init (void) |
| Function to initializes the I2S module. More... | |
| I2S_Handle | I2S_open (uint_least8_t index, I2S_Params *params) |
| Function to initialize a given I2S peripheral specified by the particular index value. The parameter specifies which mode the I2S will operate. More... | |
| void | I2S_Params_init (I2S_Params *params) |
| Function to initialize the I2S_Params struct to its defaults. More... | |
| int_fast16_t | I2S_read (I2S_Handle handle, I2S_BufDesc *desc) |
| Function to queue a buffer of data to the I2S in callback mode for reading. More... | |
| int_fast16_t | I2S_readIssue (I2S_Handle handle, I2S_BufDesc *desc) |
| Function to queue a buffer of data to the I2S in Issue/Reclaim mode for reading. More... | |
| size_t | I2S_readReclaim (I2S_Handle handle, I2S_BufDesc **pDesc) |
| Function to retrieve a full buffer of data read by the I2S. More... | |
| int_fast16_t | I2S_write (I2S_Handle handle, I2S_BufDesc *desc) |
| Function to queue a buffer of data to the I2S in callback mode for writing. More... | |
| int_fast16_t | I2S_writeIssue (I2S_Handle handle, I2S_BufDesc *desc) |
| Function to queue a buffer of data to the I2S in Issue/Reclaim mode for writing. More... | |
| size_t | I2S_writeReclaim (I2S_Handle handle, I2S_BufDesc **pDesc) |
| Function to retrieve a buffer that the I2S has finished writing. More... | |
| #define I2S_ERROR (I2S_STATUS_ERROR) |
| #define I2S_WAIT_FOREVER (~(0U)) |
Wait forever define.
| typedef struct I2S_Config_* I2S_Handle |
A handle that is returned from a I2S_open() call.
| typedef struct I2S_BufDesc_ I2S_BufDesc |
I2S buffer descriptor for issue/reclaim mode.
| typedef void(* I2S_Callback) (I2S_Handle handle, I2S_BufDesc *desc) |
The definition of a callback function used by the I2S driver when used in I2S_MODE_CALLBACK.
| I2S_Handle | I2S_Handle |
| buf | Pointer to read/write buffer |
| count | Number of elements read/written |
| typedef enum I2S_DataMode_ I2S_DataMode |
I2S mode settings.
This enum defines the read and write modes for the configured I2S.
| typedef enum I2S_OpMode_ I2S_OpMode |
I2S mode settings.
This enumeration defines the mode for I2S operation.
| typedef enum I2S_SerInActiveConfig_ I2S_SerInActiveConfig |
I2S Serializer InActive state settings.
This enumeration defines the Serializer configuration in inactive state.
| typedef enum I2S_PinMode_ I2S_PinMode |
I2S serial pin mode.
This enumeration defines the Serial pin configuration
| typedef struct I2S_Params_ I2S_Params |
Basic I2S Parameters.
I2S parameters are used to with the I2S_open() call. Default values for these parameters are set using I2S_Params_init().
| typedef void(* I2S_CloseFxn) (I2S_Handle handle) |
A function pointer to a driver specific implementation of I2S_CloseFxn().
| typedef int_fast16_t(* I2S_ControlFxn) (I2S_Handle handle, uint_fast16_t cmd, void *arg) |
A function pointer to a driver specific implementation of I2S_control().
| typedef void(* I2S_InitFxn) (I2S_Handle handle) |
A function pointer to a driver specific implementation of I2S_init().
| typedef I2S_Handle(* I2S_OpenFxn) (I2S_Handle handle, I2S_Params *params) |
A function pointer to a driver specific implementation of I2S_OpenFxn().
| typedef int_fast16_t(* I2S_IssueFxn) (I2S_Handle handle, I2S_BufDesc *desc) |
A function pointer to a driver specific implementation of I2S_IssueFxn().
| typedef size_t(* I2S_ReclaimFxn) (I2S_Handle handle, I2S_BufDesc **desc) |
A function pointer to a driver specific implementation of I2S_ReclaimFxn().
| typedef struct I2S_FxnTable_ I2S_FxnTable |
The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation.
| typedef struct I2S_Config_ I2S_Config |
I2S Global configuration.
The I2S_Config structure contains a set of pointers used to characterize the I2S driver implementation.
This structure needs to be defined before calling I2S_init() and it must not be changed thereafter.
| enum I2S_DataMode_ |
I2S mode settings.
This enum defines the read and write modes for the configured I2S.
| Enumerator | |
|---|---|
| I2S_MODE_CALLBACK |
Non-blocking and will return immediately. When the transfer by the intr is finished the configured callback function is called. |
| I2S_MODE_ISSUERECLAIM |
Use I2S_readIssue, I2S_writeIssue calls to queue buffers to the I2S. I2S_readReclaim() blocks until a buffer of data is available. I2S_writeReclaim() blocks until a buffer of data has been written and the descriptor can be returned back to the caller. |
| enum I2S_OpMode_ |
| enum I2S_PinMode_ |
| void I2S_close | ( | I2S_Handle | handle | ) |
Function to close a given I2S peripheral specified by the I2S handle.
| handle | A I2S_Handle returned from I2S_open |
| int_fast16_t I2S_control | ( | I2S_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given I2S_Handle.
Commands for I2S_control can originate from I2S.h or from implementation specific I2S*.h (I2SCC32XX.h, etc.. ) files. While commands from I2S.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific I2S*.h files add unique driver capabilities but are not API portable across all I2S driver implementations.
Commands supported by I2S.h follow a I2S_CMD_<cmd> naming convention.
Commands supported by I2S*.h follow a I2S*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See I2S_control command codes for command codes.
See I2S_control return status codes for status codes.
| handle | A I2S handle returned from I2S_open() |
| cmd | I2S.h or I2S*.h commands. |
| arg | An optional R/W (read/write) command argument accompanied with cmd |
| void I2S_init | ( | void | ) |
Function to initializes the I2S module.
| I2S_Handle I2S_open | ( | uint_least8_t | index, |
| I2S_Params * | params | ||
| ) |
Function to initialize a given I2S peripheral specified by the particular index value. The parameter specifies which mode the I2S will operate.
| index | Logical peripheral number for the I2S indexed into the I2S_config table |
| params | Pointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only). |
| void I2S_Params_init | ( | I2S_Params * | params | ) |
Function to initialize the I2S_Params struct to its defaults.
| params | An pointer to I2S_Params structure for initialization |
Defaults values are:
| params | Parameter structure to initialize |
| int_fast16_t I2S_read | ( | I2S_Handle | handle, |
| I2S_BufDesc * | desc | ||
| ) |
Function to queue a buffer of data to the I2S in callback mode for reading.
| handle | A I2S_Handle |
| desc | A pointer to a I2S_BufDesc object. The bufPtr and bufSize fields must be set to a buffer and the size of the buffer before passing to this function. |
| int_fast16_t I2S_readIssue | ( | I2S_Handle | handle, |
| I2S_BufDesc * | desc | ||
| ) |
Function to queue a buffer of data to the I2S in Issue/Reclaim mode for reading.
| handle | A I2S_Handle |
| desc | A pointer to a I2S_BufDesc object. The bufPtr and bufSize fields must be set to a buffer and the size of the buffer before passing to this function. |
| size_t I2S_readReclaim | ( | I2S_Handle | handle, |
| I2S_BufDesc ** | pDesc | ||
| ) |
Function to retrieve a full buffer of data read by the I2S.
| handle | A I2S_Handle |
| pDesc | A pointer to a I2S_BufDesc pointer. |
| int_fast16_t I2S_write | ( | I2S_Handle | handle, |
| I2S_BufDesc * | desc | ||
| ) |
Function to queue a buffer of data to the I2S in callback mode for writing.
| handle | A I2S_Handle |
| desc | A pointer to a I2S_BufDesc object. The bufPtr and bufSize fields must be set to a buffer and the size of the buffer before passing to this function. |
| int_fast16_t I2S_writeIssue | ( | I2S_Handle | handle, |
| I2S_BufDesc * | desc | ||
| ) |
Function to queue a buffer of data to the I2S in Issue/Reclaim mode for writing.
| handle | A I2S_Handle |
| desc | A pointer to a I2S_BufDesc object. The bufPtr and bufSize fields must be set to a buffer and the size of the buffer before passing to this function. |
| size_t I2S_writeReclaim | ( | I2S_Handle | handle, |
| I2S_BufDesc ** | pDesc | ||
| ) |
Function to retrieve a buffer that the I2S has finished writing.
| handle | A I2S_Handle |
| pDesc | A pointer to a I2S_BufDesc pointer. |