SimpleLink MCU SDK Driver APIs
tidrivers_cc13xx_cc26xx_3_01_01_03
|
Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver. More...
#include <RF.h>
Data Fields | |
struct { | |
uint32_t nInactivityTimeout | |
Inactivity timeout in us. More... | |
RF_Mode * pRfMode | |
Mode of operation. More... | |
RF_RadioSetup * pOpSetup | |
Radio setup radio operation, only ram right now. More... | |
uint32_t nPowerUpDuration | |
Measured poweruptime in us or specified startup time (if left default it will measure) More... | |
bool bPowerUpXOSC | |
Allways enable XOSC_HF at chip wakeup. More... | |
bool bUpdateSetup | |
Setup command update. More... | |
uint16_t nPowerUpDurationMargin | |
Powerup duration margin in us. More... | |
void * pPowerCb | |
Power up callback. More... | |
void * pErrCb | |
Error callback. More... | |
} | clientConfig |
Configuration. More... | |
struct { | |
struct { | |
rfc_CMD_FS_t cmdFs | |
FS command encapsulating FS state. More... | |
} mode_state | |
(Mode-specific) state structure More... | |
Semaphore_Struct semSync | |
Semaphore used by runCmd(), pendCmd() and powerdown sequence. More... | |
RF_EventMask volatile eventSync | |
Event mask/value used by runCmd() and waitCmd() More... | |
void * pCbSync | |
Internal storage for user callback. More... | |
RF_EventMask unpendCause | |
Return value for RF_pendCmd() More... | |
Clock_Struct clkInactivity | |
Clock used for inactivity timeouts. More... | |
Clock_Struct clkReqAccess | |
Clock used for request access timeouts. More... | |
RF_CmdHandle volatile chLastPosted | |
Command handle of most recently posted command. More... | |
bool bYielded | |
Client has indicated that there are no more commands. More... | |
} | state |
State & variables. More... | |
Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver.
uint32_t RF_Object::nInactivityTimeout |
Inactivity timeout in us.
RF_Mode* RF_Object::pRfMode |
Mode of operation.
RF_RadioSetup* RF_Object::pOpSetup |
Radio setup radio operation, only ram right now.
uint32_t RF_Object::nPowerUpDuration |
Measured poweruptime in us or specified startup time (if left default it will measure)
bool RF_Object::bPowerUpXOSC |
Allways enable XOSC_HF at chip wakeup.
bool RF_Object::bUpdateSetup |
Setup command update.
uint16_t RF_Object::nPowerUpDurationMargin |
Powerup duration margin in us.
void* RF_Object::pPowerCb |
Power up callback.
void* RF_Object::pErrCb |
Error callback.
struct { ... } RF_Object::clientConfig |
Configuration.
rfc_CMD_FS_t RF_Object::cmdFs |
FS command encapsulating FS state.
struct { ... } RF_Object::mode_state |
(Mode-specific) state structure
Semaphore_Struct RF_Object::semSync |
Semaphore used by runCmd(), pendCmd() and powerdown sequence.
RF_EventMask volatile RF_Object::eventSync |
Event mask/value used by runCmd() and waitCmd()
void* RF_Object::pCbSync |
Internal storage for user callback.
RF_EventMask RF_Object::unpendCause |
Return value for RF_pendCmd()
Clock_Struct RF_Object::clkInactivity |
Clock used for inactivity timeouts.
Clock_Struct RF_Object::clkReqAccess |
Clock used for request access timeouts.
RF_CmdHandle volatile RF_Object::chLastPosted |
Command handle of most recently posted command.
bool RF_Object::bYielded |
Client has indicated that there are no more commands.
struct { ... } RF_Object::state |
State & variables.