8.7.8.130. OnRestart()¶
GEL callback function called when the program is restarted.
Syntax
OnRestart( int nErrorCode );
Parameters
nErrorCode: 0 (zero) indicates success.
Description
If defined in a loaded GEL file, OnRestart() is called when the program is restarted.
Example
OnRestart(int nErrorCode)
{
if (nErrorCode)
{
GEL_TextOut("An error occurred while restarting. -%d-\n",,,,, nErrorCode);
}
else
{
GEL_TextOut("Restart was successful. -%d-\n",,,,, nErrorCode);
}
}