8.7.8.86. GEL_SetWaitInResetMode()¶
Sets or clears the Halt on Reset option.
Syntax
GEL_SetWaitInResetMode( integer );
Parameters
integer: Indicates the halt on reset mode
0 - Will not halt on a reset.
1 - Halts at the beginning of the reset vector once a reset has been set.
Description
This GEL function sets or clears the Halt on Reset menu option, which is used for resets that occur externally to the debugger.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Related Topics