8.7.8.11. GEL_Connect

GEL built-in function that can be called on a disconnected target to connect it.

Syntax

GEL_Connect();

Description

The function connects the target and then returns. It throws an exception if the target is already connected or fails to connect.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Related Topics

GEL_Disconnect

GEL_IsConnected