8.7.8.54. GEL_MemoryFill()¶
Fills a block of memory.
Syntax
GEL_MemoryFill( startAddress, page, length, pattern, [patternSizeType] );
Parameters
startAddress: is the first address in the block.
page: identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/0 space).
For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.
length: defines the number of words to fill.
pattern: is the value that is placed in each word in the block.
patternSizeType (optional): specifies the size of pattern that CCStudio should interpret. If not provided, pattern size will be interpreted as being the word size on the memory page on which the GEL_MemoryFill operation is taking place. Acceptable values for patternSizeType are as follows:
Target specific types: size of the type depends on the target used
0x00 - Char
0x01 - Unsigned Char
0x02 - Short
0x03 - Unsigned Short
0x04 - Enum
0x06 - Int
0x07 - Unsigned Int
0x08 - Long
0x09 - Unsigned Long
0x0B - Pointer
Target independent signed types
0x0C - 8 bit integer
0x0E - 16 bit integer
0x10 - 24 bit integer
0x12 - 32 bit integer
0x14 - 40 bit integer
0x16 - 48 bit integer
0x18 - 64 bit integer
Target independent unsigned types
0x0D - 8 bit unsigned integer
0x0F - 16 bit unsigned integer
0x11 - 24 bit unsigned integer
0x13 - 32 bit unsigned integer
0x15 - 40 bit unsigned integer
0x17 - 48 bit unsigned integer
0x19 - 64 bit unsigned integer
Large and floating point types
0x1E - long long
0x1F - unsigned long long
0x20 - float
0x22 - 32 bit IEEE single precision float
0x24 - double
0x26 - 64 bit IEEE double precision float
0x28 - long double
Description
This function can be used to fill a block of target memory with a specified pattern.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
// Fill memory 0x1000 on page 0 with 0x1000 instances of 0xa5a5 where
0xa5a5 is interpreted by CCS as a 32-bit unsigned integer.
GEL_MemoryFill(0x1000, 0, 0x100, 0xa5a5, 0x13);
Related Topics