8.7.8.57. GEL_MemoryLoadData()

Loads a block of memory from a file.

Syntax

GEL_MemoryLoadData( startAddress, page, length, "fileName" );

Parameters

startAddress: is the first address in the block.

page: identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/O space)

For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.

length: defines the number of values to load from the file

fileName: name of the file to load data from. The fileName must be enclosed in quotation marks.

Description

GEL_MemoryLoadData() is an extension to GEL_MemoryLoad() and supports loading data in additional formats to target memory from a specified file.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

GEL_MemoryLoadData( 0x100, 0 , 0x100, "c:\\mydir\\myfile.dat" );

Related Topics

GEL_MemoryListSupportedTypes

GEL_MemoryLoad

GEL_MemorySave

GEL_MemorySaveData