8.7.8.77. GEL_Run()¶
Runs code.
Syntax
GEL_Run( ["Condition"] );
Parameters
Condition (optional): specifies the condition that must be satisfied while the target is executing. Once the execution reaches a breakpoint and the condition is evaluated to be false, the CCStudio™ IDE debugger stops at that address. The condition must be enclosed in quotation marks.
Description
This function starts executing code on the target. If a condition is specified, the run function becomes a conditional run statement. That is, execution continues while the statement is true. The statement is evaluated at each breakpoint that is encountered.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_Run();
GEL_Run("A != B");
Related Topics