8.7.7. Adding GEL Functions to the Scripts Menu Using Keywords

You can add GEL functions that you access frequently to the Scripts menu of the CCStudio™ IDE menu bar. To do this, use the menuitem keyword to create a new drop-down list of menu items under the Scripts menu. You can then use the keywords hotmenu or dialog to add new menu items in the most recent drop-down list.

There is no limit to the number of GEL functions that can be defined. However, the total number of menu items that can be added under the Scripts menu is limited. The Script Commands View can be used to display all the GEL functions menu items.