8.7.8.94. GEL_SubStr¶
Return a substring of a literal string or string variable.
Syntax
GEL_SubStr( text, begin, count );
Parameters
text: is a literal string or string variable
begin: is an integer representing the starting position of the substring
count: is an integer indicating the length of the substring
Description
return a substring of text
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
string company = "Texas Instruments";
string product = "CCS"
string product_str = GEL_StrCat(company, " ", product, " ", "11.2");
int length = GEL_StrLen(product_str); // length == 26
string state = GEL_SubStr(company, 0, 5); // state == "Texas"
GEL_TextOut(product_str);
Related Topics