8.7.8.3. GEL_AdvancedReset()¶
Resets processor.
Syntax
GEL_AdvancedReset( "reset_name", [synchronous = 1] );
Parameters
reset_name: specifies the name of the reset
synchronous (optional): is an optional integer parameter (defaulted to 1) where 1 means wait for the reset to be issued before returning to GEL and 0 means queue up the reset and return to GEL immediately.
Description
This GEL function issues any possible reset other than the default reset for the connected hardware device. Since some advanced resets don't indicate when the reset is complete, there is no way for this function to wait for the reset to complete, only to wait for the reset to be issued. However, for most advanced resets, this is the same thing.
Synchronous
Synchronous from GEL: Yes unless synchronous is set to 0
Completely synchronous: Yes unless synchronous is set to 0
Related Topics