8.7.8.59. GEL_MemorySaveBin()¶
Saves a block of memory to a file in raw binary.
Syntax
GEL_MemorySaveBin( start_address, page, count, "file_path" );
Parameters
start_address: The first address in the block
page: Identifies the type of memory to save. On many targets, page zero is the only page. However, on some targets there are multiple pages identifying the different types of memory: 0 (Program memory), 1 (Data memory), or 2 (I/O space)
count: The number of words of memory to save.
file_path: Path to the file in which the data should be saved. The file_path must be enclosed in quotation marks.
Description
Save a block of target memory to a specified file in raw binary format.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_MemorySaveBin( 0x2400, 0, 100, "C:/path/to/file.bin" );
Related Topics