8.7.8.107. GEL_SyncRun¶
Performs a run operation on every target that is in the same group as the current target.
Syntax
GEL_SyncRun();
Description
Performs a run operation on every target that is in the same group as the current target. The operation performed is the same as the run command that may be invoked from the PDM debug menu.
As with the other synchronous operations, the operation is performed on all targets simultaneously.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_SyncRun( );
Related Topics