8.7.8.60. GEL_MemorySaveCoff()¶
Saves one or more blocks of memory to a file in COFF format.
Syntax
GEL_MemorySaveCoff( "file_path", page, start_address1, count1, [start_address2], [count2], ... );
Parameters
file_path: Path to the file in which the data should be saved. The file_path must be enclosed in quotation marks.
page: Identifies the type of memory to save. On many targets, page zero is the only page. However, on some targets there are multiple pages identifying the different types of memory: 0 (Program memory), 1 (Data memory), or 2 (I/O space)
start_addressN: The start address of the N-th block of memory.
countN: The number of words in the N-th block of memory.
Description
Save one or more blocks of memory to a specified file in COFF format.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_MemorySaveCoff( "C:/path/to/file.out", 0, 0x2400, 100, 0x3000, 0x40 );
Related Topics