8.7.8.46. GEL_LoadSecureDebugManager()¶
Loads the ARM Secure Debug Manager for authenticating a device using challenge vector signing.
Syntax
GEL_LoadSecureDebugManager()
Parameters
None.
Description
This function loads the Secure Debug Manager library for the current device and launches the authentication procedure that allows the user to authenticate a debug session by signing a challenge vector with security keys. It needs to be called after a connection with CS_DAP has been established. This function requires CCS user interface to complete the dialogs.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_LoadSecureDebugManager();
Related Topics