8.7.8.12. GEL_Dialog()¶
Display a dialog in CCStudio™ IDE, or other tool if supported.
Syntax
GEL_Dialog( "dialog_text", "icon_type", "default_button", "button0_text", ["button1_text"], ... );
Parameters
dialog_text: The text to be displayed in the dialog.
icon_type: The icon to be displayed in the dialog. Must be one of "EXCLAMATION", "INFORMATION", "QUESTION", or "STOP".
default_button: The index of the button to be selected by default. The buttons are index starting at 0.
buttonN_text: The text of the N-th button. There must be at least one button.
Description
Requests an interactive dialog be presented to the user. This requires support from the tool using the debugger, like CCStudio IDE. This function will block until the dialog is closed. The index of the button clicked by the user will be returned. An error will be thrown if there is no support for dialogs or if the user dismisses the dialog.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_Dialog("I am a dialog!", "INFORMATION", 0, "OK", "CANCEL")