8.7.8.5. GEL_AsmStepOver()

Steps over the next assembly instruction.

Syntax

GEL_AsmStepOver( [count] );

Parameters

count (optional): specifies the number of times the command is to be repeated. If no count is specified, steps over a single assembly instruction.

Description

In the Assembly or mixed mode, steps over a single assembly instruction. Repeats count times. If the instruction is an assembly subroutine, executes the assembly subroutine and then halts after the assembly function returns. In source mode, may not appear to move the source cursor at all.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Related Topics

GEL_SrcStepInto

GEL_SrcStepOver

GEL_AsmStepInto