8.7.8.29. GEL_GetStringTargetDbProperty

Return the value of a string driver/device property

Syntax

GEL_GetStringTargetDbProperty( propertyName );

Parameters

propertyName: specifies the property name

Description

Return the value of the property

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

int bHaltOnConnect = GEL_GetBoolTargetDbProperty("haltOnConnectByDefault");
string defConn = GEL_GetStringTargetDbProperty("DefaultConnection");
int numIntrs = GEL_GetNumericTargetDbProperty("Number of Interrupt Supported");

Related Topics

GEL_GetBoolDebugProperty

GEL_GetNumericDebugProperty

GEL_GetStringDebugProperty

GEL_GetBoolDriverProperty

GEL_GetNumericDriverProperty

GEL_GetStringDriverProperty

GEL_GetBoolTargetDbProperty

GEL_GetNumericTargetDbProperty