8.7.8.117. GEL_UnloadGel()¶
Unloads a GEL file.
Syntax
GEL_UnloadGel( "fileName" );
Parameters
fileName: names the GEL file to be unloaded. The fileName must be enclosed in quotation marks.
Description
This function unloads the functions defined in the specified GEL file.
The fileName Parameters is case sensitive. The filename must be specified exactly as it was when the file was loaded. If the file is not in the current directory, the fileName Parameters must provide the full path. A double backslash escape sequence is required to ensure that you get a backslash into the fileName Parameters.
Note: When a file is opened using menu commands, Windows capitalizes the drive letter.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_UnloadGel("C:\\MyDir\\myfile.gel");
Related Topics