8.7.8.40. GEL_IsResetSupported()¶
Queries if a reset is supported.
Syntax
GEL_IsResetSupported( "reset_name" );
Parameters
reset_name: The name of the reset.
Description
Queries if a reset with the given name is supported on this target.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_IsResetSupported("System Reset");
Related Topics