8.7.8.27. GEL_GetStringDebugProperty

Return the value of a string debug property

Syntax

GEL_GetStringDebugProperty( propertyName );

Parameters

propertyName: specifies the property name

Description

Return the value of the property

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

int autoResetOnConnect = GEL_GetBoolDebugProperty("AutoResetOnConnect");
string flashFiles = GEL_GetStringDebugProperty("FlashFiles");
int flashTimeout = GEL_GetNumericDebugProperty(""FlashTimeoutValue");

Related Topics

GEL_GetBoolDebugProperty

GEL_GetNumericDebugProperty

GEL_GetBoolDriverProperty

GEL_GetNumericDriverProperty

GEL_GetStringDriverProperty

GEL_GetBoolTargetDbProperty

GEL_GetNumericTargetDbProperty

GEL_GetStringTargetDbProperty