8.7.8.15. GEL_Disconnect

GEL built-in function that can be called on a connected target to disconnect it.

Syntax

GEL_Disconnect();

Description

The function disconnects the target and then returns. It throws an exception if the target is already disconnected or cannot be disconnected.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Related Topics

GEL_Connect

GEL_IsConnected