TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
snp.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  @file snp.h
4 
5  @brief main header file for the serial network processor
6 
7  Group: WCS, BTS
8  $Target Device: DEVICES $
9 
10  ******************************************************************************
11  $License: BSD3 2015 $
12  ******************************************************************************
13  $Release Name: PACKAGE NAME $
14  $Release Date: PACKAGE RELEASE DATE $
15  *****************************************************************************/
16 
25 #ifndef SNP_H
26 #define SNP_H
27 
28 #ifdef __cplusplus
29 extern "C"
30 {
31 #endif
32 
33 /*********************************************************************
34  * INCLUDES
35  */
36 
37 #include "hal_types.h"
38 
39 /*********************************************************************
40 * EXTERNAL VARIABLES
41 */
42 
48 /*********************************************************************
49  * CONSTANTS
50  */
51 
53 #define SNP_IMAGE_START 0x00000000
54 
56 
59 #define SNP_NPI_ASYNC_CMD_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_ASYNC<<5))
61 #define SNP_NPI_SYNC_REQ_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCREQ<<5))
63 #define SNP_NPI_SYNC_RSP_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCRSP<<5))
65 
69 // Fixed size, must not exceed 2 bits!
71 // the upper two bits of NPI frame cmd1 field is reserved for subgroup value.
73  SNP_DEVICE_GRP = 0,
74  SNP_GAP_GRP,
75  SNP_GATT_GRP,
76  SNP_RFU_GRP
77 };
78 
83 #define SNP_MASK_EVT_REQ 0x02
84 #define SNP_GET_REVISION_REQ 0x03
85 #define SNP_HCI_CMD_REQ 0x04
86 #define SNP_GET_STATUS_REQ 0x06
87 #define SNP_GET_RAND_REQ 0x07
88 #define SNP_TEST_REQ 0x10
89 
95 #define SNP_POWER_UP_IND 0x01
96 #define SNP_MASK_EVENT_RSP 0x02
97 #define SNP_GET_REVISION_RSP 0x03
98 #define SNP_HCI_CMD_RSP 0x04
99 #define SNP_EVENT_IND 0x05
100 #define SNP_GET_STATUS_RSP 0x06
101 #define SNP_SYNC_ERROR_CMD_IND 0x07
102 #define SNP_GET_RAND_RSP 0x08
103 #define SNP_TEST_RSP 0x10
104 
110 #define SNP_INIT_DEVICE_REQ 0x41
111 #define SNP_START_ADV_REQ 0x42
112 #define SNP_SET_ADV_DATA_REQ 0x43
113 #define SNP_STOP_ADV_REQ 0x44
114 #define SNP_UPDATE_CONN_PARAM_REQ 0x45
115 #define SNP_TERMINATE_CONN_REQ 0x46
116 #define SNP_SET_GAP_PARAM_REQ 0x48
117 #define SNP_GET_GAP_PARAM_REQ 0x49
118 #define SNP_SET_SECURITY_PARAM_REQ 0x4A
119 #define SNP_SEND_SECURITY_REQUEST_REQ 0x4B
120 #define SNP_SET_AUTHENTICATION_DATA_REQ 0x4C
121 #define SNP_SET_WHITE_LIST_POLICY_REQ 0x4D
122 
128 #define SNP_INIT_DEVICE_CNF 0x41
129 #define SNP_SET_ADV_DATA_CNF 0x43
130 #define SNP_UPDATE_CONN_PARAM_CNF 0x45
131 #define SNP_SET_GAP_PARAM_RSP 0x48
132 #define SNP_GET_GAP_PARAM_RSP 0x49
133 #define SNP_SET_SECURITY_PARAM_RSP 0x4A
134 #define SNP_SEND_AUTHENTICATION_DATA_RSP 0x4C
135 #define SNP_SET_WHITE_LIST_POLICY_RSP 0x4D
136 
142 #define SNP_ADD_SERVICE_REQ 0x81
143 #define SNP_ADD_CHAR_VAL_DECL_REQ 0x82
144 #define SNP_ADD_CHAR_DESC_DECL_REQ 0x83
145 #define SNP_REGISTER_SERVICE_REQ 0x84
146 #define SNP_GET_ATTR_VALUE_REQ 0x85
147 #define SNP_SET_ATTR_VALUE_REQ 0x86
148 #define SNP_CHAR_READ_CNF 0x87
149 #define SNP_CHAR_WRITE_CNF 0x88
150 #define SNP_SEND_NOTIF_IND_REQ 0x89
151 #define SNP_CCCD_UPDATED_CNF 0x8B
152 #define SNP_SET_GATT_PARAM_REQ 0x8C
153 #define SNP_GET_GATT_PARAM_REQ 0x8D
154 #define SNP_REG_PREDEF_SRV_REQ 0x8E
155 
161 #define SNP_ADD_SERVICE_RSP 0x81
162 #define SNP_ADD_CHAR_VAL_DECL_RSP 0x82
163 #define SNP_ADD_CHAR_DESC_DECL_RSP 0x83
164 #define SNP_REGISTER_SERVICE_RSP 0x84
165 #define SNP_GET_ATTR_VALUE_RSP 0x85
166 #define SNP_SET_ATTR_VALUE_RSP 0x86
167 #define SNP_CHAR_READ_IND 0x87
168 #define SNP_CHAR_WRITE_IND 0x88
169 #define SNP_SEND_NOTIF_IND_CNF 0x89
170 #define SNP_CCCD_UPDATED_IND 0x8B
171 #define SNP_SET_GATT_PARAM_RSP 0x8C
172 #define SNP_GET_GATT_PARAM_RSP 0x8D
173 #define SNP_REG_PREDEF_SRV_RSP 0x8E
174 
179 #define SNP_SUCCESS 0x00
180 #define SNP_FAILURE 0x83
181 #define SNP_INVALID_PARAMS 0x84
182 #define SNP_CMD_ALREADY_IN_PROGRESS 0x85
183 #define SNP_CMD_REJECTED 0x86
184 #define SNP_OUT_OF_RESOURCES 0x87
185 #define SNP_UNKNOWN_ATTRIBUTE 0x88
186 #define SNP_UNKNOWN_SERVICE 0x89
187 #define SNP_ALREADY_ADVERTISING 0x8A
188 #define SNP_NOT_ADVERTISING 0x8B
189 #define SNP_HCI_RSP_COLLISION_RSP 0x8C
190 #define SNP_HCI_CMD_UNKNOWN 0x8D
191 #define SNP_GATT_COLLISION 0x8E
192 #define SNP_NOTIF_IND_NOT_ENABLE_BY_CLIENT 0x8F
193 #define SNP_NOTIF_IND_NOT_ALLOWED 0x90
194 #define SNP_NOTIF_IND_NO_CCCD_ATTRIBUTE 0x91
195 #define SNP_NOT_CONNECTED 0x92
196 #define SNP_FAILURE_NO_ATT_RSP 0x93
197 
204 #define SNP_CONN_EST_EVT 0x0001
205 #define SNP_CONN_TERM_EVT 0x0002
206 #define SNP_CONN_PARAM_UPDATED_EVT 0x0004
207 #define SNP_ADV_STARTED_EVT 0x0008
208 #define SNP_ADV_ENDED_EVT 0x0010
209 #define SNP_ATT_MTU_EVT 0x0020
210 #define SNP_SECURITY_EVT 0x0040
211 #define SNP_AUTHENTICATION_EVT 0x0080
212 #define SNP_ERROR_EVT 0x8000
213 
216 #define SNP_DEV_ALL_EVENT_MASK (SNP_CONN_EST_EVT | SNP_CONN_TERM_EVT | \
218 SNP_CONN_PARAM_UPDATED_EVT | SNP_ADV_STARTED_EVT | SNP_ADV_ENDED_EVT | \
219  SNP_ATT_MTU_EVT | SNP_ERROR_EVT)
220 
221 /* HCI Opcodes */
225 #define SNP_HCI_OPCODE_EXT_SET_TX_POWER 0xFC01
226 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_TX 0xFC08
227 #define SNP_HCI_OPCODE_EXT_MODEM_HOP_TEST_TX 0xFC09
228 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_RX 0xFC0A
229 #define SNP_HCI_OPCODE_EXT_END_MODEM_TEST 0xFC0B
230 #define SNP_HCI_OPCODE_EXT_SET_BDADDR 0xFC0C
231 #define SNP_HCI_OPCODE_EXT_SET_SCA 0xFC0D
232 #define SNP_HCI_OPCODE_EXT_ENABLE_PTM 0xFC0E
233 #define SNP_HCI_OPCODE_EXT_SET_MAX_DTM_TX_POWER 0xFC11
234 #define SNP_HCI_OPCODE_EXT_RESET_SYSTEM 0xFC1D
235 #define SNP_HCI_OPCODE_READ_BDADDR 0x1009
236 #define SNP_HCI_OPCODE_READ_RSSI 0x1405
237 #define SNP_HCI_OPCODE_LE_RECEIVER_TEST 0x201D
238 #define SNP_HCI_OPCODE_LE_TRANSMITTER_TEST 0x201E
239 #define SNP_HCI_OPCODE_LE_TEST_END 0x201F
240 #define SNP_HCI_OPCODE_EXT_PER 0xFC14
241 #define SNP_HCI_OPCODE_EXT_DECRYPT 0xFC05
242 #define SNP_HCI_OPCODE_LE_ENCRYPT 0x2017
243 #define SNP_HCI_OPCODE_EXT_OVERRIDE_SL 0xFC1A
244 #define SNP_HCI_OPCODE_EXT_SET_FAST_TX_RESP_TIME 0xFC07
245 #define SNP_HCI_OPCODE_EXT_ONE_PKT_PER_EVT 0xFC02
246 #define SNP_HCI_OPCODE_EXT_GET_CONNECTION_INFO 0xFC20
247 
251 #define SNP_HCI_OPCODE_SIZE 0x02
253 
254 
255 /* Advertising */
259 #define SNP_ADV_TYPE_CONN 0x00
260 #define SNP_ADV_TYPE_SCANABLE 0x02
261 #define SNP_ADV_TYPE_NONCONN 0x03
262 
269 #define SNP_FILTER_POLICY_ALL 0x00
270 #define SNP_FILTER_POLICY_WHITE 0x03
271 
278 #define SNP_ADV_STOP_ON_CONN 0x00
280 #define SNP_ADV_RESTART_ON_CONN_EST 0x01
283 #define SNP_ADV_RESTART_ON_CONN_TERM 0x02
286 
293 #define SNP_SCANRSP_DATA 0x00 // Scan response data
295 #define SNP_NONCONN_ADV_DATA 0x01 // Non-connectable advertising data.
297 #define SNP_CONN_ADV_DATA 0x02 // Connectable advertising data.
299 
303 #define SNP_MAX_ADVDATA_LENGTH 31
305 
307 
310 #define SNP_CT_SUPERVISOR_TO 0x08
311 #define SNP_CT_PEER_REQ 0x13
312 #define SNP_CT_HOST_REQ 0x16
313 #define SNP_CT_CTRL_PKT_TO 0x22
314 #define SNP_CT_CTRL_PKT_INST_PASS 0x28
315 #define SNP_CT_LSTO_VIOLATION 0x3B
316 #define SNP_CT_MIC_FAILURE 0x3D
317 
321 /* Connection Parameters and Updates */
322 #define SNP_CONN_INT_MIN 0x0006
324 #define SNP_CONN_INT_MAX 0x0C80
325 
326 #define SNP_CONN_SL_MIN 0x0000
328 #define SNP_CONN_SL_MAX 0x01F3
329 
330 #define SNP_CONN_SUPERVISOR_TIMEOUT_MIN 0x000A
332 #define SNP_CONN_SUPERVISOR_TIMEOUT_MAX 0x0C80
333 
334 
337 #define SNP_PRIMARY_SERVICE 1
339 #define SNP_SECONDARY_SERVICE 2
341 
343 #define SNP_CHAR_MANAGED_BY_AP 0x00
344 #define SNP_CHAR_MANAGED_BY_NP 0x01
345 
346 
349 #define SNP_16BIT_UUID_SIZE 2
350 #define SNP_128BIT_UUID_SIZE 16
351 
356 #define SNP_GATT_PERMIT_READ 0x01
359 #define SNP_GATT_PERMIT_WRITE 0x02
361 #define SNP_GATT_PERMIT_AUTHEN_READ 0x04
363 #define SNP_GATT_PERMIT_AUTHEN_WRITE 0x08
365 #define SNP_GATT_PERMIT_ENCRYPT_READ 0x40
367 #define SNP_GATT_PERMIT_ENCRYPT_WRITE 0x80
369 
372 #define SNP_GATT_PERM_RFU_MASK (SNP_GATT_PERMIT_READ | \
374  SNP_GATT_PERMIT_WRITE | \
375  SNP_GATT_PERMIT_AUTHEN_READ | \
376  SNP_GATT_PERMIT_AUTHEN_WRITE | \
377  SNP_GATT_PERMIT_ENCRYPT_READ | \
378  SNP_GATT_PERMIT_ENCRYPT_WRITE)
379 
383 #define SNP_GATT_PROP_READ 0x0002
384 #define SNP_GATT_PROP_WRITE_NORSP 0x0004
385 #define SNP_GATT_PROP_WRITE 0x0008
386 #define SNP_GATT_PROP_NOTIFICATION 0x0010
387 #define SNP_GATT_PROP_INDICATION 0x0020
388 
390 #define SNP_GATT_CHAR_MAX_LENGTH 512
392 
396 #define SNP_SEND_NOTIFICATION 0x01
398 #define SNP_SEND_INDICATION 0x02
400 
406 #define SNP_GGS_SERV_ID 0x01
407 #define SNP_DIS_SERV_ID 0x02
408 
413 #define SNP_DEVINFO_SYSTEM_ID 0
414 #define SNP_DEVINFO_MODEL_NUMBER 1
415 #define SNP_DEVINFO_SERIAL_NUMBER 2
416 #define SNP_DEVINFO_FIRMWARE_REV 3
417 #define SNP_DEVINFO_HARDWARE_REV 4
418 #define SNP_DEVINFO_SOFTWARE_REV 5
419 #define SNP_DEVINFO_MANUFACTURER_NAME 6
420 #define SNP_DEVINFO_11073_CERT_DATA 7
421 #define SNP_DEVINFO_PNP_ID 8
422 
423 #define SNP_DEVINFO_SYSTEM_ID_LEN 8
425 
427 #define SNP_DEVINFO_PNP_ID_LEN 7
428 
430 // this is for information only, do not change it here.
431 #define SNP_DEVINFO_STRING_LEN 21
432 
437 #define SNP_GGS_DEVICE_NAME_ATT 0
438 #define SNP_GGS_APPEARANCE_ATT 1
439 #define SNP_GGS_PERI_PRIVACY_FLAG_ATT 2
440 #define SNP_GGS_RECONNCT_ADDR_ATT 3
441 #define SNP_GGS_PERI_CONN_PARAM_ATT 4
442 #define SNP_GGS_PERI_PRIVACY_FLAG_PROPS 5
443 #define SNP_GGS_W_PERMIT_DEVICE_NAME_ATT 6
444 #define SNP_GGS_W_PERMIT_APPEARANCE_ATT 7
445 #define SNP_GGS_W_PERMIT_PRIVACY_FLAG_ATT 8
446 
447 #define SNP_GAP_DEVICE_NAME_LEN 21
449 
450 // Privacy Flag States
451 #define SNP_GAP_PRIVACY_DISABLED 0x00
452 #define SNP_GAP_PRIVACY_ENABLED 0x01
453 
454 
459 #define SNP_DESC_HEADER_GEN_SHORT_UUID 0x01
460 #define SNP_DESC_HEADER_GEN_LONG_UUID 0x02
461 #define SNP_DESC_HEADER_CCCD 0x04
462 #define SNP_DESC_HEADER_FORMAT 0x08
463 #define SNP_DESC_HEADER_USER_DESC 0x80
464 #define SNP_DESC_HEADER_UNSUPPORTED_MASK 0x70
465 
467 #define SNP_GATT_CLIENT_CFG_NOTIFY 0x0001
468 #define SNP_GATT_CLIENT_CFG_INDICATE 0x0002
469 
470 
473 #define SNP_RESPONSE_NOT_NEEDED 0x00
474 #define SNP_RESPONSE_NEEDED 0x01
475 
477 #define SNP_INVALID_HANDLE 0x0000
478 
479 
483 #define SNP_GAP_TERM_CONN_DEFAULT 0x00
484 #define SNP_GAP_TERM_CONN_IMMEDIATLY 0x01
485 
490 #define SNP_GAPBOND_PAIRING_MODE 0x00
491 #define SNP_GAPBOND_IO_CAPABILITIES 0x01
492 #define SNP_GAPBOND_BONDING_ENABLED 0x02
493 #define SNP_GAPBOND_ERASE_ALLBONDS 0x03
494 #define SNP_GAPBOND_LRU_BOND_REPLACEMENT 0x04
495 
500 #define SNP_GAPBOND_PAIRING_STATE_COMPLETE 0x01
501 #define SNP_GAPBOND_PAIRING_STATE_BONDED 0x02
502 #define SNP_GAPBOND_PAIRING_STATE_BOND_SAVED 0x03
503 
507 /*-------------------------------------------------------------------
508 * TYPEDEFS - Initialization and Configuration
509 */
510 /*** Device Data Types ***/
511 
523 PACKED_TYPEDEF_STRUCT
524 {
525  uint16_t eventMask;
529 
537 PACKED_TYPEDEF_STRUCT
538 {
539  uint16_t maskedEvent;
543 
551 PACKED_TYPEDEF_STRUCT
552 {
553  uint16_t memAlo;
554  uint16_t memMax;
555  uint16_t memSize;
557 
565 PACKED_TYPEDEF_STRUCT
566 {
567  uint16_t opcode;
568  uint8_t *pData;
576 
584 PACKED_TYPEDEF_STRUCT
585 {
586  uint8_t status;
587  uint16_t opcode;
588  uint8_t *pData;
595 
603 PACKED_TYPEDEF_STRUCT
604 {
605  uint8_t status;
606  uint16_t snpVer;
607  uint8_t stackBuildVer[10];
609 
617 PACKED_TYPEDEF_STRUCT
618 {
619  uint32_t rand;
621 
627 PACKED_TYPEDEF_STRUCT
628 {
629  uint8_t gapRoleStatus;
630  uint8_t advStatus;
634  uint8_t ATTstatus;
638  uint8_t ATTmethod;
643 
644 /*** GAP Data Types ***/
645 
653 PACKED_TYPEDEF_STRUCT
654 {
655  uint8_t type;
656  uint16_t timeout;
657  uint16_t interval;
660  uint8_t filterPolicy;
664  uint8_t initiatorAddress[6];
665  uint8_t behavior;
667 
668 
678 PACKED_TYPEDEF_STRUCT
679 {
680  uint8_t type;
681  uint8_t *pData;
683 
693 PACKED_TYPEDEF_STRUCT
694 {
695  uint16_t connHandle;
696  uint8_t option;
698 
706 PACKED_TYPEDEF_STRUCT
707 {
708  uint16_t connHandle;
709  uint16_t intervalMin;
710  uint16_t intervalMax;
716  uint16_t slaveLatency;
722  uint16_t supervisionTimeout;
725 
731 
741 PACKED_TYPEDEF_STRUCT
742 {
743  uint8_t status;
744  uint16_t connHandle;
746 
780 PACKED_TYPEDEF_STRUCT
781 {
782  uint16_t paramId;
783  uint16_t value;
785 
795 PACKED_TYPEDEF_STRUCT
796 {
797  uint8_t status;
798  uint16_t paramId;
799  uint16_t value;
801 
813 PACKED_TYPEDEF_STRUCT
814 {
815  uint32_t authData;
817 
818 /*** GATT Data Types ***/
819 
827 PACKED_TYPEDEF_STRUCT
828 {
829  uint8_t type;
830  uint8_t UUID[16];
836 
857 PACKED_TYPEDEF_STRUCT
858 {
859  uint8_t charValPerms;
860  uint16_t charValProps;
861  uint8_t mgmtOption;
862  uint16_t charValMaxLen;
863  uint8_t UUID[16];
871 
879 PACKED_TYPEDEF_STRUCT
880 {
881  uint8_t status;
882  uint16_t attrHandle;
884 
899 PACKED_TYPEDEF_STRUCT
900 {
901  uint8_t perms;
903 
913 PACKED_TYPEDEF_STRUCT
914 {
915  uint8_t format;
916  uint8_t exponent;
917  uint16_t unit;
918  uint8_t namespace;
919  uint16_t desc;
921 
931 PACKED_TYPEDEF_STRUCT
932 {
933  uint8_t perms;
934  uint16_t maxLen;
935  uint16_t initLen;
936  uint8_t *pDesc;
938 
948 PACKED_TYPEDEF_STRUCT
949 {
950  uint8_t perms;
951  uint16_t maxLen;
952  uint8_t UUID[2];
956 
966 PACKED_TYPEDEF_STRUCT
967 {
968  uint8_t perms;
969  uint16_t maxLen;
970  uint8_t UUID[16];
974 
995 PACKED_TYPEDEF_STRUCT
996 {
997  uint8_t header;
1004 
1015 PACKED_TYPEDEF_STRUCT
1016 {
1017  uint8_t status;
1018  uint8_t header;
1019  uint16_t handles[6];
1024 
1032 PACKED_TYPEDEF_STRUCT
1033 {
1034  uint8_t status;
1035  uint16_t startHandle;
1036  uint16_t endHandle;
1038 
1046 PACKED_TYPEDEF_STRUCT
1047 {
1048  uint16_t connHandle;
1049  uint16_t attrHandle;
1050  uint16_t offset;
1051  uint16_t maxSize;
1053 
1061 PACKED_TYPEDEF_STRUCT
1062 {
1063  uint8_t status;
1064  uint16_t connHandle;
1065  uint16_t attrHandle;
1066  uint16_t offset;
1067  uint8_t *pData;
1070 
1080 PACKED_TYPEDEF_STRUCT
1081 {
1082  uint16_t connHandle;
1083  uint16_t attrHandle;
1084  uint8_t rspNeeded;
1085  uint16_t offset;
1086  uint8_t *pData;
1089 
1109 PACKED_TYPEDEF_STRUCT
1110 {
1111  uint8_t status;
1112  uint16_t connHandle;
1114 
1120 PACKED_TYPEDEF_STRUCT
1121 {
1122  uint16_t connHandle;
1123  uint16_t attrHandle;
1124  uint8_t authenticate;
1125  uint8_t type;
1126  uint8_t *pData;
1128 
1197 PACKED_TYPEDEF_STRUCT
1198 {
1199  uint8_t status;
1203 
1219 PACKED_TYPEDEF_STRUCT
1220 {
1221  uint8_t serviceID;
1222  uint8_t paramID;
1225  uint8_t *pData;
1227 
1235 PACKED_TYPEDEF_STRUCT
1236 {
1237  uint16_t attrHandle;
1238  uint8_t *pData;
1240 
1248 PACKED_TYPEDEF_STRUCT
1249 {
1250  uint8_t status;
1251  uint16_t attrHandle;
1253 
1261 PACKED_TYPEDEF_STRUCT
1262 {
1263  uint16_t attrHandle;
1265 
1273 PACKED_TYPEDEF_STRUCT
1274 {
1275  uint8_t status;
1276  uint16_t attrHandle;
1277  uint8_t *pData;
1279 
1287 PACKED_TYPEDEF_STRUCT
1288 {
1289  uint8_t serviceID;
1290  uint8_t paramID;
1292 
1302 PACKED_TYPEDEF_STRUCT
1303 {
1304  uint16_t connHandle;
1305  uint16_t cccdHandle;
1306  uint8_t rspNeeded;
1307  uint16_t value;
1309 
1317 PACKED_TYPEDEF_STRUCT
1318 {
1319  uint8_t useWhiteList;
1321 
1326 typedef union
1327 {
1328  //Mask events
1331 
1332  //Revision
1334 
1335  //Rand
1337 
1338  //HCI
1341 
1342  //Status
1344 
1345  //Test
1347 
1348  //Advertising
1351  snpSetAdvDataCnf_t setAdvDataCnf;
1352 
1353  //Connection
1357 
1358  //GAP Parameters
1360  snpSetGapParamRsp_t setGapParamRsp;
1361  snpGetGapParamReq_t getGapParamReq;
1363 
1364  //Security
1365  snpSetSecParamReq_t setSecParamReq;
1366  snpSetSecParamRsp_t setSecParamRsp;
1368  snpSetAuthDataRsp_t setAuthDataRsp;
1369 
1370  //White List
1372  snpSetWhiteListRsp_t setWhiteListRsp;
1373 
1374  //Services
1376  snpAddServiceRsp_t addServiceRsp;
1382 
1383  //Incoming GATT Requests
1389  snpNotifIndCnf_t notifIndCnf;
1390 
1391  //NP GATT Parameters of predefined services
1395  snpGetGattParamRsp_t getGattParamRsp;
1396 
1397  //CCCD Updates
1399  snpCharCfgUpdatedRsp_t charcfgUpdatedRsp;
1400 } snp_msg_t;
1401 
1402 /*** SNP EVENTS ***/
1403 
1413 PACKED_TYPEDEF_STRUCT
1414 {
1415  uint16_t connHandle;
1416  uint16_t connInterval;
1417  uint16_t slaveLatency;
1419  uint8_t addressType;
1420  uint8_t pAddr[6];
1421 } snpConnEstEvt_t;
1422 
1432 PACKED_TYPEDEF_STRUCT
1433 {
1434  uint16_t connHandle;
1435  uint8_t reason;
1437 
1447 PACKED_TYPEDEF_STRUCT
1448 {
1449  uint16_t connHandle;
1450  uint16_t connInterval;
1451  uint16_t slaveLatency;
1454 
1464 PACKED_TYPEDEF_STRUCT
1465 {
1466  uint8_t status;
1468 
1478 PACKED_TYPEDEF_STRUCT
1479 {
1480  uint8_t state;
1481  uint8_t status;
1483 
1493 PACKED_TYPEDEF_STRUCT
1494 {
1495  uint16_t opcode;
1496  uint8_t status;
1497 } snpErrorEvt_t;
1498 
1508 PACKED_TYPEDEF_STRUCT
1509 {
1510  uint16_t connHandle;
1511  uint16_t attMtuSize;
1513 
1523 PACKED_TYPEDEF_STRUCT
1524 {
1525  uint8_t display;
1526  uint8_t input;
1527  uint32_t numCmp;
1529 
1534 typedef union
1535 {
1544 } snpEventParam_t;
1545 
1553 PACKED_TYPEDEF_STRUCT
1554 {
1555  uint16_t event;
1557 } snpEvt_t;
1558 
1568 typedef struct
1569 {
1570  uint16_t intervalMin;
1571  uint16_t intervalMax;
1572  uint16_t latency;
1573  uint16_t timeout;
1575 
1578 /*********************************************************************
1579  * MACROS
1580  */
1581 
1586 #define SNP_CMD1_HDR_MASK 0xC0
1588 
1590 #define SNP_CMD1_HDR_POS 0x6
1591 
1593 #define SNP_GET_OPCODE_HDR_CMD1(cmd) (((cmd) & SNP_CMD1_HDR_MASK) >> SNP_CMD1_HDR_POS)
1594 
1596 #define SNP_CMD1_ID_MASK 0x3F
1597 
1599 #define SNP_GET_OPCODE_ID_CMD1(cmd) ((cmd) & SNP_CMD1_ID_MASK)
1600 
1603 /*********************************************************************
1604 *********************************************************************/
1605 
1606 #ifdef __cplusplus
1607 }
1608 #endif
1609 
1610 #endif /* SNP_H */
1611 
Parameter Structure for the ATT MTU size updated Event data.
Definition: snp.h:1508
uint16_t offset
2 Byte Offset of the characteristic to start writing to
Definition: snp.h:1085
uint8_t addressType
1 Byte Type of initiator address
Definition: snp.h:1419
Parameter Structure for the Error Event SNP_ERROR_EVT.
Definition: snp.h:1493
uint8_t perms
1 Byte Permissions of the attribute, see GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:950
uint16_t intervalMax
2 Byte
Definition: snp.h:1571
uint8_t status
1 Byte Status of the request list of status generated by the SNP.
Definition: snp.h:1496
Parameter Structure for SNP_updateConnParam.
Definition: snp.h:706
uint8_t perms
1 Byte Permissions of the attribute, see GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:968
Parameter Structure for the Security Event.
Definition: snp.h:1478
Parameter Structure for SNP_CHAR_READ_IND / @ ref SNP_charRead.
Definition: snp.h:1046
snpEventParam_t * pEvtParams
snpEventParam_t
Definition: snp.h:1556
snpGetRevisionRsp_t revisionRsp
Get revision Response.
Definition: snp.h:1333
uint16_t connInterval
2 Byte
Definition: snp.h:1450
Parameter Structure for the Characteristic Configuration Update Indication.
Definition: snp.h:1302
uint8_t * pData
Pointer to.
Definition: snp.h:1126
uint8_t status
1 Byte Command Status (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1199
snpSetGattParamRsp_t setGattParamRsp
Set GATT parameter response.
Definition: snp.h:1393
snpAddCharDescDeclRsp_t addCharDescDeclRsp
Add characteristic descriptor Response.
Definition: snp.h:1380
uint16_t timeout
2 Byte
Definition: snp.h:1573
struct snpCharWriteCnf_t snpNotifIndCnf_t
Parameter Structure for SNP_sendNotifcnf_rsp - Same Structure as snpCharWriteCnf_t.
snpGetGattParamReq_t getGattParamReq
Get GATT parameter response.
Definition: snp.h:1394
uint8_t initiatorAddrType
1 Byte Initiator Address Type, Reserved for Future Use
Definition: snp.h:663
Connection parameters for the peripheral device.
Definition: snp.h:1568
snpGetRandRsp_t randRsp
Get Random Number Response.
Definition: snp.h:1336
snpHciCmdRsp_t hciCmdRsp
HCI command response (event)
Definition: snp.h:1340
snpConnEstEvt_t connEstEvt
Parameter Structure snpConnEstEvt_t.
Definition: snp.h:1536
Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP.
Definition: snp.h:1219
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_REQ.
Definition: snp.h:1287
Parameter Structure for the Characteristic Write Request Indication data.
Definition: snp.h:1080
snpRegisterServiceRsp_t registerService
Register service Response.
Definition: snp.h:1381
snpUpdateConnParamReq_t updateConnParamsReq
Update connection parameters indication.
Definition: snp.h:1355
uint16_t startHandle
2 Byte First attribute handle of the registered service
Definition: snp.h:1035
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1276
uint16_t charValMaxLen
Definition: snp.h:862
uint8_t behavior
1 Byte Behavior of Advertisement on connection event, Adv. behavior when connection are established o...
Definition: snp.h:665
snpAddAttrUserDesc_t * pUserDesc
Pointer to Parameter Structure, snpAddAttrUserDesc_t.
Definition: snp.h:1002
snpSetGapParamReq_t setGapParamReq
Set GAP parameter Request.
Definition: snp.h:1359
uint16_t maxLen
Definition: snp.h:969
Parameter Structure for SNP_UPDATE_CONN_PARAM_CNF.
Definition: snp.h:741
uint16_t opcode
2 Byte HCI opcode that was executed in the request, list of all HCI commands allowed by the SNP...
Definition: snp.h:587
Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ.
Definition: snp.h:813
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1275
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1449
uint16_t connInterval
2 Byte
Definition: snp.h:1416
snpAddCharValueDeclReq_t addCharValueDecReq
Add characteristic value Request.
Definition: snp.h:1377
uint16_t charValProps
2 Byte property of the value attribute, see GATT Characteristic Properties Bit Fields ...
Definition: snp.h:860
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being read
Definition: snp.h:1065
uint8_t useWhiteList
1 Byte White List Filter Policy, Advertisement Filter Policy Type
Definition: snp.h:1319
snpSetSecParamRsp_t setSecParamRsp
Set Security Requirements response.
Definition: snp.h:1366
snpAddAttrGenLongUUID_t * pLongUUID
Pointer to Parameter Structure, snpAddAttrGenLongUUID_t.
Definition: snp.h:999
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1064
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1082
uint8_t perms
1 Byte permissions of the attribute, GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:901
struct snpSetGattParamRsp_t snpAddServiceRsp_t
1 Byte Command Status Response
uint8_t charValPerms
1 Byte permissions of the value attribute, see GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:859
snpSetGapParamRsp_t setGapParamRsp
Set GAP parameter Response.
Definition: snp.h:1360
Parameter Structure for the Connection Established Event.
Definition: snp.h:1413
snpSetGattParamReq_t setGattParamReq
Set GATT parameter request.
Definition: snp.h:1392
snpCharReadCnf_t readCnf
Characteristic read confirmation.
Definition: snp.h:1385
struct snpSetGattParamReq_t snpGetGattParamRsp_t
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_RSP.
Parameter Structure for SNP_writeCharCnf / SNP_CHAR_WRITE_CNF.
Definition: snp.h:1109
uint8_t type
1 Byte Type of Advertisement, see Advertisement Type
Definition: snp.h:655
uint8_t * pData
Pointer of Data to write/retrieved.
Definition: snp.h:1225
snpGetGattParamRsp_t getGattParamRsp
Get GATT parameter request.
Definition: snp.h:1395
uint32_t rand
32-bit Random Number generated by TRNG
Definition: snp.h:619
Parameter Structure for the Connection terminated Event.
Definition: snp.h:1432
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1048
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1237
snpMaskEventRsp_t maskEventCnf
event mask confirmation.
Definition: snp.h:1330
snpTermConnReq_t connTermReq
Connection terminated Request.
Definition: snp.h:1354
uint16_t unit
2 Byte Unit, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:917
uint16_t paramId
2 Byte GAP Parameter ID, GAP Parameter IDs
Definition: snp.h:798
uint16_t connHandle
2 Byte Connection Handle to terminate
Definition: snp.h:695
uint8_t * pData
Definition: snp.h:588
struct snpSetGattParamRsp_t snpSetGapParamRsp_t
1 Byte Command Status Response
Parameter Structure for SNP_addDescriptionValue.
Definition: snp.h:995
snpUpdateConnParamCnf_t updateConnParamsCnf
Update connection parameters, request.
Definition: snp.h:1356
snpNotifIndCnf_t notifIndCnf
Indication Confirmation.
Definition: snp.h:1389
uint8_t state
1 Byte New Security State Security States
Definition: snp.h:1480
Parameter Structure for the Advertising state change Event.
Definition: snp.h:1464
Parameter Structure used to add a generic attribute descriptor (long UUID)
Definition: snp.h:966
snpAdvStatusEvt_t advStatusEvt
Parameter Structure snpAdvStatusEvt_t.
Definition: snp.h:1539
Parameter Structure used to add a Format attribute.
Definition: snp.h:913
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP.
Definition: snp.h:1015
Parameter Structure for MITM Authentication data to be displayed.
Definition: snp.h:1523
uint16_t value
2 Byte Value to write to the CCCD
Definition: snp.h:1307
SNP Event Parameters.
Definition: snp.h:1534
uint8_t exponent
1 Byte Exponent, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:916
uint8_t paramID
1 Byte ID of the parameter to retrieved.
Definition: snp.h:1290
uint8_t header
1 Byte Header Field, SNP GATT Descriptors Header
Definition: snp.h:997
uint16_t memMax
2 Byte maximum HEAP ever allocated since startup
Definition: snp.h:554
uint8_t input
1 Byte TRUE if device must input passcode.
Definition: snp.h:1526
struct snpSetGattParamRsp_t snpSetWhiteListRsp_t
1 Byte Command Status Response
uint8_t authenticate
1 Byte Reserved for future use
Definition: snp.h:1124
snpAuthenticationEvt_t authenticationEvt
Parameter Structure snpAuthenticationEvt_t.
Definition: snp.h:1543
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1415
uint8_t type
1 Byte Type of the service to add. see Service Type
Definition: snp.h:829
snpStartAdvReq_t startAdv
Start advertising request.
Definition: snp.h:1349
uint8_t rspNeeded
1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field ...
Definition: snp.h:1306
uint16_t maxLen
Definition: snp.h:951
Parameter Structure for the response to SNP_getRev.
Definition: snp.h:617
uint16_t offset
2 Byte Offset of the characteristic to start reading from
Definition: snp.h:1066
uint8_t option
1 Byte Type of disconnection requested. see GAP GATT Terminate connection request option field...
Definition: snp.h:696
snpUpdateConnParamEvt_t updateConnParamEvt
Parameter Structure snpUpdateConnParamEvt_t.
Definition: snp.h:1538
Parameter Structure for SNP_registerService / SNP_REGISTER_SERVICE_RSP.
Definition: snp.h:1032
uint16_t cccdHandle
2 Byte Handle of the characteristic value attribute to notify/indicate
Definition: snp.h:1305
snpCharCfgUpdatedInd_t charCfgUpdatedReq
Characteristic configuration updated indication.
Definition: snp.h:1398
snpAddAttrGenShortUUID_t * pShortUUID
Pointer to Parameter Structure, snpAddAttrGenShortUUID_t.
Definition: snp.h:998
snpHciCmdReq_t hciCmdReq
HCI command request.
Definition: snp.h:1339
Parameter Structure for the Update Connection Parameter Event.
Definition: snp.h:1447
uint16_t maxLen
2 Byte Maximum possible length of the string, plus one byte for null terminator (range from 1 to 512)...
Definition: snp.h:934
uint16_t intervalMin
2 Byte
Definition: snp.h:1570
Parameter Structure for SNP_CHAR_READ_CNF / snpCharReadCnf_t.
Definition: snp.h:1061
snpCharWriteInd_t charWriteInd
Characteristic write request.
Definition: snp.h:1386
uint8_t gapRoleStatus
1 Byte Current state of the GAP Role ( gaprole_States_t)
Definition: snp.h:629
struct snpSetGapParamReq_t snpGetGapParamReq_t
Parameter Structure for SNP_getGapParam / SNP_GET_GAP_PARAM_REQ - Same Structure as snpSetGapParamReq...
uint16_t attMtuSize
2 Byte New ATT MTU Size negotiated between GATT client and GATT server.
Definition: snp.h:1511
snpCharWriteCnf_t charWriteCnf
Characteristic write confirmation.
Definition: snp.h:1387
struct snpCharWriteCnf_t snpCharCfgUpdatedRsp_t
Parameter Structure for SNP_processCharConfigUpdatedCnf / SNP_CCCD_UPDATED_CNF - Same Structure as sn...
uint8_t display
1 Byte TRUE if device must display passcode.
Definition: snp.h:1525
uint16_t slaveLatency
2 Byte
Definition: snp.h:1417
uint8_t status
1 Byte Status list of status generated by the SNP.
Definition: snp.h:1466
snpErrorEvt_t advErrorEvt
Parameter Structure snpErrorEvt_t.
Definition: snp.h:1541
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:797
snpAddCharValueDeclRsp_t addCharValueDecRsp
Add characteristic value Response.
Definition: snp.h:1378
uint8_t status
status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:743
Parameter Structure used for SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_REQ.
Definition: snp.h:857
1 Byte Command Status Response
Definition: snp.h:1197
snpTestCmdRsp_t testCmdRsp
Test command response.
Definition: snp.h:1346
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1263
uint8_t status
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:605
struct snpSetGapParamReq_t snpSetSecParamReq_t
Parameter Structure for SNP_setSecurityParams / SNP_SET_SECURITY_PARAM_REQ - Same Structure as snpSet...
Parameter Structure used to add a Client Characteristic Configuration Description Attribute...
Definition: snp.h:899
uint16_t opcode
2 Byte SNP opcode that triggered the error
Definition: snp.h:1495
uint16_t value
2 Byte Parameter Value set if for SET command
Definition: snp.h:783
uint16_t connHandle
handle of the connection the parameter update was intended for
Definition: snp.h:744
uint8_t * pData
Pointer of data value to set.
Definition: snp.h:1238
snpAddAttrFormat_t * pFormat
Pointer to Parameter Structure, snpAddAttrFormat_t.
Definition: snp.h:1001
snpSetWhiteListReq_t setWhiteListReq
Set the White List Filter Policy request.
Definition: snp.h:1371
SNP_CMD1_HDR_TYPE
list of subgroup
Definition: snp.h:72
uint16_t timeout
2 Byte Timeout of the advertisement.
Definition: snp.h:656
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1434
uint8_t serviceID
1 Byte ID of the service containing the parameter to define
Definition: snp.h:1289
Add Service Request Structure for SNP_addService / SNP_ADD_SERVICE_REQ.
Definition: snp.h:827
snpSecurityEvt_t securityEvt
Parameter Structure snpSecurityEvt_t.
Definition: snp.h:1542
Parameter Structure for SNP_maskEvt.
Definition: snp.h:523
uint16_t opcode
Definition: snp.h:567
snpSetAdvDataCnf_t setAdvDataCnf
Set advertising data Response.
Definition: snp.h:1351
uint16_t connHandle
2 Byte handle of the connection to update parameters to.
Definition: snp.h:708
Parameter Structure for SNP_setWhiteListFilterPolicy / SNP_SET_WHITE_LIST_POLICY_REQ.
Definition: snp.h:1317
Parameter Structure for SNP_MASK_EVENT_RSP.
Definition: snp.h:537
uint16_t memSize
2 Byte total HEAP size
Definition: snp.h:555
uint8_t rspNeeded
1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field ...
Definition: snp.h:1084
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1112
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1250
uint16_t memAlo
2 Byte HEAP allocated memory
Definition: snp.h:553
struct snpSetGattParamRsp_t snpSetAuthDataRsp_t
1 Byte Command Status Response
uint16_t event
2 Byte Event, list of asynchronous events generated by the SNP.
Definition: snp.h:1555
Parameter Structure for Response to SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_RSP.
Definition: snp.h:879
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being written
Definition: snp.h:1083
uint8_t mgmtOption
1 Byte Reserved for future use
Definition: snp.h:861
struct snpSetGattParamRsp_t snpSetSecParamRsp_t
1 Byte Command Status Response
uint16_t snpVer
2 Byte Version of the SNP (major, minor)
Definition: snp.h:606
uint8_t * pData
Pointer to the advertisement data buffer to update, up to 31 Bytes.
Definition: snp.h:681
uint32_t numCmp
32 bit Numeric Comparison value to display, 0 if not used.
Definition: snp.h:1527
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1034
uint16_t maskedEvent
Definition: snp.h:539
Parameter Structure used to add a generic attribute descriptor (short UUID)
Definition: snp.h:948
uint8_t status
1 Byte Status upon entering this state list of status generated by the SNP.
Definition: snp.h:1481
Parameter Structure for the Characteristic Notification and Indication Request data This is a packed ...
Definition: snp.h:1120
uint8_t status
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:586
uint16_t value
2 Byte Parameter Value retrieved.
Definition: snp.h:799
snpGetGapParamRsp_t getGapParamRsp
Get GAP parameter Response.
Definition: snp.h:1362
snpSetAuthDataReq_t setAuthDataReq
Set Authentication Data request.
Definition: snp.h:1367
uint8_t type
1 Byte Type of Advertisement data to update, see Adv. data buffer
Definition: snp.h:680
uint16_t attrHandle
2 Byte Attribute handle of the characteristic value.
Definition: snp.h:1251
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute to notify/indicate
Definition: snp.h:1123
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1063
snpSetAuthDataRsp_t setAuthDataRsp
Set Authentication Data response.
Definition: snp.h:1368
uint16_t intervalMin
2 Byte Minimum value for the connection event interval.
Definition: snp.h:709
uint8_t serviceID
Definition: snp.h:1221
uint8_t reason
1 Byte Reason of the termination connection termination reason.
Definition: snp.h:1435
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.
Definition: snp.h:780
uint8_t * pData
Pointer to data of the value to set.
Definition: snp.h:1277
uint16_t latency
2 Byte
Definition: snp.h:1572
snpGetStatusCmdRsp_t getStatusRsp
Get status Response.
Definition: snp.h:1343
uint16_t offset
2 Byte Offset of the characteristic to start reading from
Definition: snp.h:1050
snpGetGapParamReq_t getGapParamReq
Get GAP parameter Request.
Definition: snp.h:1361
uint8_t perms
1 Byte Permissions of the attribute, GATT Attribute Access Permissions Bit Fields, force to Read only
Definition: snp.h:933
Connection Termination Request Structure.
Definition: snp.h:693
uint16_t supervisionTimeout
2 Byte
Definition: snp.h:1452
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1122
snpSetAdvDataReq_t setAdvDataReq
Set advertising data Request.
Definition: snp.h:1350
uint16_t desc
< 1 Byte Namespace, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:918
uint8_t status
1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:1111
uint8_t header
Definition: snp.h:1018
SNP Event Structure.
Definition: snp.h:1553
Parameter Structure for the Get GAP Parameter Value Response.
Definition: snp.h:795
Parameter Structure for SNP_getAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1261
uint8_t status
1 Byte Command Status list of status generated by the SNP.
Definition: snp.h:1017
uint16_t endHandle
2 Byte Last attribute handle of the registered service
Definition: snp.h:1036
snpAddServiceRsp_t addServiceRsp
Add service response.
Definition: snp.h:1376
Parameter Structure for response to SNP_setAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1248
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1304
snpAddAttrCccd_t * pCCCD
Pointer to Parameter Structure, snpAddAttrCccd_t.
Definition: snp.h:1000
The SNP message. A union of all SNP message types.
Definition: snp.h:1326
uint16_t attrHandle
2 Byte Handle of the characteristic value attribute being read
Definition: snp.h:1049
snpSetWhiteListRsp_t setWhiteListRsp
Set the White List Filter Policy response.
Definition: snp.h:1372
uint16_t maxSize
2 Byte Max Size of the data to read
Definition: snp.h:1051
uint8_t status
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:881
struct snpSetGattParamRsp_t snpSetAdvDataCnf_t
1 Byte Command Status Response
snpATTMTUSizeEvt_t attMTUSizeEvt
Parameter Structure snpATTMTUSizeEvt_t.
Definition: snp.h:1540
Parameter Structure for SNP_startAdv.
Definition: snp.h:653
Parameter Structure for SNP_getRev.
Definition: snp.h:603
uint16_t connHandle
2 Byte Handle of the connection
Definition: snp.h:1510
uint32_t authData
4 Byte Authentication Data. 000000 - 999999 or TRUE/FALSE
Definition: snp.h:815
snpAddServiceReq_t addServiceReq
Add service request.
Definition: snp.h:1375
uint8_t format
1 Byte Format, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:915
uint16_t attrHandle
2 Byte attribute handle of the characteristic value.
Definition: snp.h:882
uint8_t * pData
Definition: snp.h:1086
uint16_t paramId
2 Byte GAP Parameter ID, GAP Parameter IDs or snpSetSecParamReq_t
Definition: snp.h:782
snpAddCharDescDeclReq_t addCharDescDeclReq
Add characteristic descriptor Request.
Definition: snp.h:1379
Parameter Structure for response to SNP_getAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1273
Parameter Structure for SNP_setAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1235
Parameter Structure for SNP_HCI_CMD_RSP.
Definition: snp.h:584
uint8_t * pData
Definition: snp.h:1067
Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Pa...
Definition: snp.h:627
snpMaskEventReq_t maskEventReq
event mask request.
Definition: snp.h:1329
Parameter Structure for SNP_setAdvData.
Definition: snp.h:678
snpCharCfgUpdatedRsp_t charcfgUpdatedRsp
Characteristic configuration update response.
Definition: snp.h:1399
snpConnTermEvt_t connTermEvt
Parameter Structure snpConnTermEvt_t.
Definition: snp.h:1537
uint16_t initLen
2 Byte initial length of the string, plus one byte for null terminator (must be <= snpAddAttrUserDesc...
Definition: snp.h:935
snpCharReadInd_t readInd
Characteristic read request.
Definition: snp.h:1384
uint8_t * pDesc
Pointer to initial string (must be null terminated)
Definition: snp.h:936
uint16_t eventMask
Definition: snp.h:525
uint8_t type
1 Byte Type of the request, see SNP indication type
Definition: snp.h:1125
Parameter Structure used to add a User Descriptor attribute.
Definition: snp.h:931
snpSetSecParamReq_t setSecParamReq
Set the Security Requirements request.
Definition: snp.h:1365
Parameter Structure for SNP_executeHCIcmd.
Definition: snp.h:565
snpNotifIndReq_t notifIndReq
Notification or indication request.
Definition: snp.h:1388
uint16_t supervisionTimeout
2 Byte
Definition: snp.h:1418
Parameter Structure for SNP_executeTestCmd.
Definition: snp.h:551
uint16_t slaveLatency
2 Byte
Definition: snp.h:1451
Copyright 2017, Texas Instruments Incorporated