TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpCharCfgUpdatedInd_t Struct Reference

Parameter Structure for the Characteristic Configuration Update Indication. More...

Data Fields

uint16_t cccdHandle
 2 Byte Handle of the characteristic value attribute to notify/indicate
 
uint16_t connHandle
 2 Byte Handle of the connection
 
uint8_t rspNeeded
 1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field
 
uint16_t value
 2 Byte Value to write to the CCCD
 

Detailed Description

Parameter Structure for the Characteristic Configuration Update Indication.

The SNP_CCCD_UPDATED_IND event generates this.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated