TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpGetGattParamReq_t Struct Reference

Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_REQ. More...

Data Fields

uint8_t paramID
 1 Byte ID of the parameter to retrieved.
 
uint8_t serviceID
 1 Byte ID of the service containing the parameter to define
 

Detailed Description

Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_REQ.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated