TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpSecurityEvt_t Struct Reference

Parameter Structure for the Security Event. More...

Data Fields

uint8_t state
 1 Byte New Security State Security States
 
uint8_t status
 1 Byte Status upon entering this state list of status generated by the SNP.
 

Detailed Description

Parameter Structure for the Security Event.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated