TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpAddAttrUserDesc_t Struct Reference

Parameter Structure used to add a User Descriptor attribute. More...

Data Fields

uint16_t initLen
 2 Byte initial length of the string, plus one byte for null terminator (must be <= snpAddAttrUserDesc_t::maxLen)
 
uint16_t maxLen
 2 Byte Maximum possible length of the string, plus one byte for null terminator (range from 1 to 512)
 
uint8_t * pDesc
 Pointer to initial string (must be null terminated)
 
uint8_t perms
 1 Byte Permissions of the attribute, GATT Attribute Access Permissions Bit Fields, force to Read only
 

Detailed Description

Parameter Structure used to add a User Descriptor attribute.

Used with snpAddCharDescDeclReq_t

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated