TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpRegisterServiceRsp_t Struct Reference

Parameter Structure for SNP_registerService / SNP_REGISTER_SERVICE_RSP. More...

Data Fields

uint16_t endHandle
 2 Byte Last attribute handle of the registered service
 
uint16_t startHandle
 2 Byte First attribute handle of the registered service
 
uint8_t status
 1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
 

Detailed Description

Parameter Structure for SNP_registerService / SNP_REGISTER_SERVICE_RSP.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated