TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpAuthenticationEvt_t Struct Reference

Parameter Structure for MITM Authentication data to be displayed. More...

Data Fields

uint8_t display
 1 Byte TRUE if device must display passcode.
 
uint8_t input
 1 Byte TRUE if device must input passcode.
 
uint32_t numCmp
 32 bit Numeric Comparison value to display, 0 if not used.
 

Detailed Description

Parameter Structure for MITM Authentication data to be displayed.

See SNP Event Indication for more information.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated